2017-12-28 01:32 AM
I want to write IAP for STM32F030C8. I have searched through the web but found the application using Standard peripheral library. Is there any application that is developed with HAL library? Also there is no provision in STM32Cube for generating this application. Anybody have an idea for same?
#iap-for-stm32f030c8-using-hal2017-12-28 06:17 AM
You might perhaps need to code or port things
Likely to be a few examples under the HAL project trees
Repository\STM32Cube_FW_F0_V1.9.0\Projects\STM32091C_EVAL\Applications\IAP