I2S problem to change MCU from STM32F107 to STM32F407
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-04-06 11:41 AM
I developed an application using the I2S module on STM32F107VCT6.
I'm using the MikroE compiller and there aren't any library for this. Then I configured each register accordong to the Reference manual (RM0008).
Now I changed the MCU to the STM32F407VET6. I made the hardware changes on some supply pins.
As I saw on its Reference manual (RM0090), the configurations are the same, but the modulo doesn't work.
This is my code (I only added the configuration for PLLI2SN and PLLI2SR registers). If you retire this and use in a STM32F107 MCU, it will work well.
I'm checking the PLLI2S2 clk on MCO2 output pin and it is ok.
//BCK and LRCLK (WS) pins
GPIO_Set_Pin_Mode(&GPIOB_BASE, _GPIO_PINMASK_10 | _GPIO_PINMASK_12, _GPIO_CFG_MODE_OUTPUT | _GPIO_CFG_MODE_ALT_FUNCTION | _GPIO_CFG_SPEED_MAX);
// SD pin
GPIO_Digital_Input(&GPIOC_IDR, _GPIO_PINMASK_3);
// MCLK - systemclock
GPIO_Set_Pin_Mode(&GPIOC_BASE, _GPIO_PINMASK_6, _GPIO_CFG_MODE_OUTPUT | _GPIO_CFG_MODE_ALT_FUNCTION | _GPIO_CFG_SPEED_MAX);
// SPI2 = 1 (spi2 clock enable)
RCC_APB1ENR.SPI2EN = 1;
// PLLI2SN = 258
RCC_PLLI2SCFGR.PLLI2SNx0 = 0;
RCC_PLLI2SCFGR.PLLI2SNx1 = 1;
RCC_PLLI2SCFGR.PLLI2SNx2 = 0;
RCC_PLLI2SCFGR.PLLI2SNx3 = 0;
RCC_PLLI2SCFGR.PLLI2SNx4 = 0;
RCC_PLLI2SCFGR.PLLI2SNx5 = 0;
RCC_PLLI2SCFGR.PLLI2SNx6 = 0;
RCC_PLLI2SCFGR.PLLI2SNx7 = 0;
RCC_PLLI2SCFGR.PLLI2SNx8 = 1;
// PLLI2SR = 3
RCC_PLLI2SCFGR.PLLI2SRx0 = 1;
RCC_PLLI2SCFGR.PLLI2SRx1 = 1;
RCC_PLLI2SCFGR.PLLI2SRx2 = 0;
// I2SDIV = 3
SPI2_I2SPR.I2SDIV0 = 1;
SPI2_I2SPR.I2SDIV1 = 1;
SPI2_I2SPR.I2SDIV2 = 0;
SPI2_I2SPR.I2SDIV3 = 0;
SPI2_I2SPR.I2SDIV4 = 0;
SPI2_I2SPR.I2SDIV5 = 0;
SPI2_I2SPR.I2SDIV6 = 0;
SPI2_I2SPR.I2SDIV7 = 0;
// I2SODD = 1
SPI2_I2SPR.ODD = 1; // para o STM32F407
// CKPOL = 0
SPI2_I2SCFGR.CKPOL = 0;
// MCKOE = 1
SPI2_I2SPR.MCKOE = 1;
// SMOD = 1 (seleciona modo I2S)
SPI2_I2SCFGR.I2SMOD = 1;
// I2SSTD = 00 (I2S Phipils standard)
SPI2_I2SCFGR.I2SSTD0 = 0;
SPI2_I2SCFGR.I2SSTD1 = 0;
// PCMSYNC = 0
SPI2_I2SCFGR.PCMSYNC = 0;
// CHLEN = 1 (32 bits no pacote total)
SPI2_I2SCFGR.CHLEN = 1;
// DATLEN = 01 (24 bits de dados)
SPI2_I2SCFGR.DATLEN0 = 1;
SPI2_I2SCFGR.DATLEN1 = 0;
// CFG = 10 (MASTER TRANSMIT) OU 11 (MASTER RECEIVE)
SPI2_I2SCFGR.I2SCFG0 = 1;
SPI2_I2SCFGR.I2SCFG1 = 1;
// interrupção de recebimento enable
SPI2_CR2.RXNEIE = 1;
NVIC_IntEnable(IVT_INT_SPI2);
// I2SE = 1 (enable I2S2)
SPI2_I2SCFGR.I2SE = 1;
RCC_CR.HSEON = 1; // HSE ON
RCC_PLLCFGR.PLLSRC = 1; // HSE como fonte para PLL e PLLI2S
RCC_CR.PLLON = 1; // PLL ON
RCC_CR.PLLI2SON = 1; // PLLI2S ON
RCC_CFGR.I2SSRC = 0; // PLLI2S como fonte para I2S
while(!RCC_CR.PLLRDY); // aguarda PLL
while(!RCC_CR.PLLI2SRDY); // aguarda PLLI2S
Regards...- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-04-06 2:51 PM
And so do you see any signals at the pins? What exactly is the failure more you're reporting?
Is there some code that configures the AF mode of the specific pins? ie GPIO_PinAFConfig() in the SPLUp vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-04-07 4:24 AM
Hi,
The pins (Clock, data, left/right and clock aux) are floating.I'm using the PCM1803A for audio ADC converter.If I use this code with the MCU STM32F107, without the configuration for PLLI2SN and PLLI2SR (because it is specificaly for STM32F407)... it works wellThe diference for this two models is that the STM32F4 MCU has a dedicated clock (PLLI2SCLK). I configured this and put this clock on MCO2 output to check this (this MCU has this function). This is ok (about 86MHz for DIV = 3, ODD = 1, MCKE = 1, FS = 48kHz).It is a little strange...- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-04-07 6:29 AM
Hi Gabriel,
If no signal on pads, I would suspect the GPIO cell.FYI GPIO cell in STM32F4 family is different from STM32F1 family.Cheers,- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-04-07 8:00 AM
Hi, thanks.
I think the MikroE command are the same, like this (PB12 and PB13 as clock output):GPIO_Clk_Enable(&GPIOB_BASE);GPIO_Config(&GPIOB_BASE, (_GPIO_PINMASK_12 | _GPIO_PINMASK_13), (_GPIO_CFG_MODE_OUTPUT | _GPIO_CFG_MODE_ALT_FUNCTION | _GPIO_CFG_SPEED_MAX | _GPIO_CFG_OTYPE_PP));The MCU is working with keypad, display... and everything is ok... But I'm checking this.Regards.