cancel
Showing results for 
Search instead for 
Did you mean: 

I2S Master has Full Duplex DMA L/R Swapped after Restart

john gassel
Associate III
Posted on January 02, 2018 at 22:53

I have an application using an STM32F429ZI processor and I'm seeing a strange problem where the L/R audio output gets swapped after changing I2S frequencies.

My procedure to change frequencies is as follows:

HAL_I2S_DMAStop(&hi2s3);

HAL_I2S_DeInit(&hi2s3);

hi2s3.Init.AudioFreq = sampling_rate;

HAL_StatusTypeDef result = HAL_I2S_Init( &hi2s3);

I2SEx_TransmitReceive_DMA_DB();

//my own function above is called, which is similar to the following but instead has call to 

//HAL_DMAEx_MultiBufferStart_IT(&hi2s3, &DummyAudioOutBuf, &DummyAudioOutBuf, AUDIO_OUT_BUF_SIZE);

It doesn't always happen.  I'd say that it gets swapped about 10% of the time.  I've seen people who have similar problems when running a slave, but with the ST configured as the master, I'm surprised to see this.

Here is my I2S3 configuration:

hi2s3.Instance = SPI3;

hi2s3.Init.Mode = I2S_MODE_MASTER_TX;

hi2s3.Init.Standard = I2S_STANDARD_PHILIPS;

hi2s3.Init.DataFormat = I2S_DATAFORMAT_16B;

hi2s3.Init.MCLKOutput = I2S_MCLKOUTPUT_DISABLE;

hi2s3.Init.AudioFreq = I2S_AUDIOFREQ_16K;

hi2s3.Init.CPOL = I2S_CPOL_LOW;

hi2s3.Init.ClockSource = I2S_CLOCK_PLL;

hi2s3.Init.FullDuplexMode = I2S_FULLDUPLEXMODE_ENABLE;

#swap #stm32f4 #i2s #dma
This discussion is locked. Please start a new topic to ask your question.
20 REPLIES 20