I2C problems with STM32L Discovery
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-07-10 9:25 AM
Posted on July 10, 2015 at 18:25
I am trying to communicate with a ADT7410 I2C temperature sensor using a STM32L Discovery Board (PB6 for SCL and PB7 for SDA).
I configure the I2C with the following code:void I2C_initialization(void){ I2C_InitTypeDef I2C_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; /* Enable I2C and GPIO clocks */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE); /* Configure I2C pins: SCL and SDA */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_Init(GPIOB, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_I2C1); GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_I2C1); /* I2C configuration */ I2C_InitStructure.I2C_Mode = I2C_Mode_I2C; I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2; I2C_InitStructure.I2C_OwnAddress1 = 0x00; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitStructure.I2C_ClockSpeed = 100000; /* I2C Peripheral Enable */ I2C_Cmd(I2C1, ENABLE); /* Apply I2C configuration after enabling it */ I2C_Init(I2C1, &I2C_InitStructure);}To read data from the sensor I use the following procedure call (with parameter reg_adrs 0x04):uint16_t I2C_read2bytes(uint8_t reg_adrs) { uint8_t I2C_MSB, I2C_LSB; uint16_t I2C_total; while(I2C_GetFlagStatus(I2C1, I2C_FLAG_BUSY)); /* Send START condition */ I2C_GenerateSTART(I2C1, ENABLE); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); I2C_Send7bitAddress(I2C1, 0x48 << 1, I2C_Direction_Transmitter); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); I2C_SendData(I2C1, reg_adrs); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED)); I2C_GenerateSTART(I2C1, ENABLE); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT)); I2C_Send7bitAddress(I2C1, (0x48 << 1) | (0x01), I2C_Direction_Receiver); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED)); I2C_MSB = I2C_ReceiveData(I2C1); while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_RECEIVED)); I2C_GenerateSTOP(I2C1, ENABLE); I2C_total = (uint16_t)(I2C_MSB); return I2C_total; }However what I get in return is the decimal number 145 (0b10010001) that is the address byte I send with the second I2C_Send7bitAddress function and not the byte the slave device sends (that is however wront, that is not the byte it should return).
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0