i2c example stm32f103 data transfer format
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-03-20 2:01 AM
Posted on March 20, 2015 at 10:01
Dear all,
I am new to stm32 and i am trying to make my stm32f103 nucleo communicate with an other stm32f within the cubef1 is a nice working example:I2C_TwoBoards_ComIT i have only 1 problem with this part of the code:/* While the I2C in reception process, user can transmit data through ''aTxBuffer'' buffer */
uint8_t aTxBuffer[] =
''I send this''
;
while
(HAL_I2C_Master_Transmit_DMA(&I2cHandle, (uint16_t)I2C_ADDRESS, (uint8_t*)aTxBuffer, TXBUFFERSIZE)!= HAL_OK)
{
/* Error_Handler() function is called when Timeout error occurs.
When Acknowledge failure occurs (Slave don't acknowledge its address)
Master restarts communication */
if
(HAL_I2C_GetError(&I2cHandle) != HAL_I2C_ERROR_AF)
{
Error_Handler();
}
}
however the only data you send over the i2c lines are text converted to binary, which means you cant send all sorts of bytes.
is there a way to make the format of data I send to hexadecimal or decimal?
#example #i2c #stm32f103
Labels:
- Labels:
-
I2C
-
STM32F1 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0