2011-09-30 01:17 AM
Hello,
I've got a problem communicating with a X9258 poti via I2C. This Poti has a protocol like:Start, Adress, send Byte, read two Bytes, Stopso is it possible with the build in I2C hardware to switch between tranmitting and recieving without sending a second start?Regards, Mike2011-09-30 02:37 AM
''a X9258 poti''
You mean this:
http://www.intersil.com/data/fn/fn8168.pdf
?