2019-02-27 11:57 PM
Hi,
I use I2C like this
uint16_t I2cAddrTemp = 0x90;
uint8_t I2cWritedata = 0x00;
uint8_t I2cReaddata = 0xFF;
uint8_t read_i2c_temp(void)
{
hi2c1_status = HAL_I2C_Master_Transmit(&hi2c1, I2cAddrTemp, &I2cWritedata, 1, 1000);
//PRINTF("I2c = %02X",hi2c1_status);
hi2c1_status = HAL_I2C_Master_Receive(&hi2c1, I2cAddrTemp, &I2cReaddata, 1, 1000);
if (hi2c1_status == HAL_OK)
{
PRINTF("I2C temp = %d\n\r",(int8_t)I2cReaddata);
}
else
{
PRINTF("I2C ERROR\n\r",hi2c1_status);
}
return 0;
}And i want to use IT instead
So i change for that :
uint16_t I2cAddrTemp = 0x90;
uint8_t I2cWritedata = 0x00;
uint8_t I2cReaddata = 0xFF;
void read_i2c_temp(void)
{
HAL_I2C_Master_Transmit_IT(&hi2c1, I2cAddrTemp, &I2cWritedata, 1);
}
void HAL_I2C_MasterTxCpltCallback(I2C_HandleTypeDef *hi2c)
{
PRINTF("I2C temp TX OK\n\r");
HAL_I2C_Master_Receive_IT(&hi2c1, I2cAddrTemp, &I2cReaddata, 1);
}
void HAL_I2C_MasterRxCpltCallback(I2C_HandleTypeDef *hi2c)
{
PRINTF("I2C temp = %d\n\r",(int8_t)I2cReaddata);
}I had this lign in the HAL_I2C_MspInit function
HAL_NVIC_EnableIRQ(I2C1_IRQn);And this one in HAL_I2C_MspDeInit
HAL_NVIC_DisableIRQ(I2C1_IRQn);But I2C freeze in this configuration. Someone found a mistake?
EDIT 1 : not only I2C everything freeze.
I have 2 USART on my project.
One use DMA, the other is in direct mode.
EDIT 2 :
I found the solution
Had this code somewhere (me in mlm32l0xx_it.c)
in the .c
extern I2C_HandleTypeDef hi2c1;
/**
* @brief This function handles I2C1 event global interrupt / I2C1 wake-up interrupt through EXTI line 23.
*/
void I2C1_IRQHandler(void)
{
/* USER CODE BEGIN I2C1_IRQn 0 */
/* USER CODE END I2C1_IRQn 0 */
if (hi2c1.Instance->ISR & (I2C_FLAG_BERR | I2C_FLAG_ARLO | I2C_FLAG_OVR)) {
HAL_I2C_ER_IRQHandler(&hi2c1);
} else {
HAL_I2C_EV_IRQHandler(&hi2c1);
}
/* USER CODE BEGIN I2C1_IRQn 1 */
/* USER CODE END I2C1_IRQn 1 */
}
don't forget the .h
void I2C1_IRQHandler(void);And i change the priority in HAL_I2C_MspInit
HAL_NVIC_SetPriority(I2C1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(I2C1_IRQn);