cancel
Showing results for 
Search instead for 
Did you mean: 

I want to use the VCP capability for debugging.

CArena
Associate II

I'm using the NUCLEO-303K8 board but I have the STM link/v2 and v3 to use too if that works better. I'm working inside the STMCubeIDE. The documentation that you can call up from within the application doesn't look like it matches the application, which makes it hard to follow the directions applicable to VCP stuff.

Is there an example project that shows the VCP use that i can try out for that feature?

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1