2021-04-05 7:46 PM
I used HAL_I2C_MASTER_Transmit/Receive
The transmission function put a delay using the for statement as shown below.
HAL_StatusTypeDef HAL_I2C_Master_Transmit(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint8_t *pData, uint16_t Size, uint32_t Timeout)
{
uint32_t tickstart;
if (hi2c->State == HAL_I2C_STATE_READY)
{
/* Process Locked */
__HAL_LOCK(hi2c);
/* Init tickstart for timeout management*/
tickstart = HAL_GetTick();
if (I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_BUSY, SET, I2C_TIMEOUT_BUSY, tickstart) != HAL_OK)
{
return HAL_ERROR;
}
hi2c->State = HAL_I2C_STATE_BUSY_TX;
hi2c->Mode = HAL_I2C_MODE_MASTER;
hi2c->ErrorCode = HAL_I2C_ERROR_NONE;
/* Prepare transfer parameters */
hi2c->pBuffPtr = pData;
hi2c->XferCount = Size;
hi2c->XferISR = NULL;
/* Send Slave Address */
/* Set NBYTES to write and reload if hi2c->XferCount > MAX_NBYTE_SIZE and generate RESTART */
if (hi2c->XferCount > MAX_NBYTE_SIZE)
{
hi2c->XferSize = MAX_NBYTE_SIZE;
I2C_TransferConfig(hi2c, DevAddress, (uint8_t)hi2c->XferSize, I2C_RELOAD_MODE, I2C_GENERATE_START_WRITE);
}
else
{
hi2c->XferSize = hi2c->XferCount;
I2C_TransferConfig(hi2c, DevAddress, (uint8_t)hi2c->XferSize, I2C_AUTOEND_MODE, I2C_GENERATE_START_WRITE);
}
for(volatile uint32_t i =0; i<1000; i++)
{
}
while (hi2c->XferCount > 0U)
{
for(volatile uint32_t i =0; i<1000; i++)
{
}
/* Wait until TXIS flag is set */
if (I2C_WaitOnTXISFlagUntilTimeout(hi2c, Timeout, tickstart) != HAL_OK)
{
return HAL_ERROR;
}
/* Write data to TXDR */
hi2c->Instance->TXDR = *hi2c->pBuffPtr;
/* Increment Buffer pointer */
hi2c->pBuffPtr++;
hi2c->XferCount--;
hi2c->XferSize--;
if ((hi2c->XferCount != 0U) && (hi2c->XferSize == 0U))
{
/* Wait until TCR flag is set */
if (I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_TCR, RESET, Timeout, tickstart) != HAL_OK)
{
return HAL_ERROR;
}
if (hi2c->XferCount > MAX_NBYTE_SIZE)
{
hi2c->XferSize = MAX_NBYTE_SIZE;
I2C_TransferConfig(hi2c, DevAddress, (uint8_t)hi2c->XferSize, I2C_RELOAD_MODE, I2C_NO_STARTSTOP);
}
else
{
hi2c->XferSize = hi2c->XferCount;
I2C_TransferConfig(hi2c, DevAddress, (uint8_t)hi2c->XferSize, I2C_AUTOEND_MODE, I2C_NO_STARTSTOP);
}
}
//osDelay(1);
}
/* No need to Check TC flag, with AUTOEND mode the stop is automatically generated */
/* Wait until STOPF flag is set */
if (I2C_WaitOnSTOPFlagUntilTimeout(hi2c, Timeout, tickstart) != HAL_OK)
{
return HAL_ERROR;
}
/* Clear STOP Flag */
__HAL_I2C_CLEAR_FLAG(hi2c, I2C_FLAG_STOPF);
/* Clear Configuration Register 2 */
I2C_RESET_CR2(hi2c);
hi2c->State = HAL_I2C_STATE_READY;
hi2c->Mode = HAL_I2C_MODE_NONE;
/* Process Unlocked */
__HAL_UNLOCK(hi2c);
return HAL_OK;
}
else
{
return HAL_BUSY;
}
}
However, receive function is not delayed in the same way.
I checked with the oscilloscope, when the I2C_TransferConfig function is executed, the SLAVE address and data are taken before the FOR statement is executed.
The I2C_TransferConfig function is ambiguous to modify because it is a function that modify the CR2 register.
Is there any way to apply the delay between the slave address and the data when receiving via i2c communication?