cancel
Showing results for 
Search instead for 
Did you mean: 

I want to change to hal lib because the old source has already been created.

Study Yahoo
Associate III
Posted on November 13, 2017 at 04:07

hi 12864L LCD sample source is being applied.

I want to change to hal lib because the old source has already been created.

Help!

//-------------------------------------------------------------------------------------------------

// Universal KS0108 driver library

// STM32 MCU low-level driver

// (c) Rados³aw Kwiecieñ,

mailto:radek@dxp.pl

//-------------------------------------------------------------------------------------------------

#include 'main.h'

#define KS0108_PORT GPIOE

#define KS0108_RS GPIO_Pin_8

#define KS0108_RW GPIO_Pin_9

#define KS0108_EN GPIO_Pin_10

#define KS0108_CS1 GPIO_Pin_11

#define KS0108_CS2 GPIO_Pin_12

#define KS0108_CS3 GPIO_Pin_13

#define KS0108_D0 0

#define DISPLAY_STATUS_BUSY 0x80

extern unsigned char screen_x;

extern unsigned char screen_y;

LL_GPIO_InitTypeDef GPIO_InitStructure;

//-------------------------------------------------------------------------------------------------

// Delay function /for 8MHz/

//-------------------------------------------------------------------------------------------------

void GLCD_Delay(void)

{

asm('nop');asm('nop');asm('nop');asm('nop');

}

//-------------------------------------------------------------------------------------------------

// Enalbe Controller (0-2)

//-------------------------------------------------------------------------------------------------

void GLCD_EnableController(unsigned char controller)

{

switch(controller){

case 0 : GPIO_ResetBits(KS0108_PORT, KS0108_CS1); break;

case 1 : GPIO_ResetBits(KS0108_PORT, KS0108_CS2); break;

case 2 : GPIO_ResetBits(KS0108_PORT, KS0108_CS3); break;

}

}

//-------------------------------------------------------------------------------------------------

// Disable Controller (0-2)

//-------------------------------------------------------------------------------------------------

void GLCD_DisableController(unsigned char controller)

{

switch(controller){

case 0 : GPIO_SetBits(KS0108_PORT, KS0108_CS1); break;

case 1 : GPIO_SetBits(KS0108_PORT, KS0108_CS2); break;

case 2 : GPIO_SetBits(KS0108_PORT, KS0108_CS3); break;

}

}

//-------------------------------------------------------------------------------------------------

// Read Status byte from specified controller (0-2)

//-------------------------------------------------------------------------------------------------

unsigned char GLCD_ReadStatus(unsigned char controller)

{

unsigned char status;

GPIO_StructInit(&GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pin = 0xFF << KS0108_D0;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;

GPIO_Init(KS0108_PORT, &GPIO_InitStructure);

GPIO_SetBits(KS0108_PORT, KS0108_RW);

GPIO_ResetBits(KS0108_PORT, KS0108_RS);

GLCD_EnableController(controller);

GLCD_Delay();

GPIO_SetBits(KS0108_PORT, KS0108_EN);

GLCD_Delay();

status = ((GPIO_ReadInputData(KS0108_PORT) >> KS0108_D0) & 0xFF);

GPIO_ResetBits(KS0108_PORT, KS0108_EN);

GLCD_DisableController(controller);

return status;

}

//-------------------------------------------------------------------------------------------------

// Write command to specified controller

//-------------------------------------------------------------------------------------------------

void GLCD_WriteCommand(unsigned char commandToWrite, unsigned char controller)

{

while(GLCD_ReadStatus(controller)&DISPLAY_STATUS_BUSY);

GPIO_StructInit(&GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pin = (0xFF << KS0108_D0);

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

GPIO_Init(KS0108_PORT, &GPIO_InitStructure);

GPIO_ResetBits(KS0108_PORT, KS0108_RS | KS0108_RW);

GLCD_Delay();

GLCD_EnableController(controller);

GLCD_Delay();

GPIO_SetBits(KS0108_PORT, (commandToWrite << KS0108_D0));

commandToWrite ^= 0xFF;

GPIO_ResetBits(KS0108_PORT, (commandToWrite << KS0108_D0));

GLCD_Delay();

GPIO_SetBits(KS0108_PORT, KS0108_EN);

GLCD_Delay();

GPIO_ResetBits(KS0108_PORT, KS0108_EN);

GLCD_Delay();

GLCD_DisableController(controller);

}

//-------------------------------------------------------------------------------------------------

// Read data from current position

//-------------------------------------------------------------------------------------------------

unsigned char GLCD_ReadData(void)

{

unsigned char tmp;

while(GLCD_ReadStatus(screen_x / 64)&DISPLAY_STATUS_BUSY);

GPIO_StructInit(&GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pin = 0xFF << KS0108_D0;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;

GPIO_Init(KS0108_PORT, &GPIO_InitStructure);

GPIO_SetBits(KS0108_PORT, KS0108_RS | KS0108_RW);

GLCD_EnableController(screen_x / 64);

GLCD_Delay();

GPIO_SetBits(KS0108_PORT, KS0108_EN);

GLCD_Delay();

tmp = ((GPIO_ReadInputData(KS0108_PORT) >> KS0108_D0) & 0xFF);

GPIO_ResetBits(KS0108_PORT, KS0108_EN);

GLCD_DisableController(screen_x / 64);

screen_x++;

return tmp;

}

//-------------------------------------------------------------------------------------------------

// Write data to current position

//-------------------------------------------------------------------------------------------------

void GLCD_WriteData(unsigned char dataToWrite)

{

while(GLCD_ReadStatus(screen_x / 64)&DISPLAY_STATUS_BUSY);

GPIO_StructInit(&GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pin = (0xFF << KS0108_D0);

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

GPIO_Init(KS0108_PORT, &GPIO_InitStructure);

GPIO_ResetBits(KS0108_PORT, KS0108_RW);

GLCD_Delay();

GPIO_SetBits(KS0108_PORT, KS0108_RS);

GLCD_Delay();

GPIO_SetBits(KS0108_PORT, (dataToWrite << KS0108_D0));

dataToWrite ^= 0xFF;

GPIO_ResetBits(KS0108_PORT, (dataToWrite << KS0108_D0));

GLCD_Delay();

GLCD_EnableController(screen_x / 64);

GLCD_Delay();

GPIO_SetBits(KS0108_PORT, KS0108_EN);

GLCD_Delay();

GPIO_ResetBits(KS0108_PORT, KS0108_EN);

GLCD_Delay();

GLCD_DisableController(screen_x / 64);

screen_x++;

}

//-------------------------------------------------------------------------------------------------

//

//-------------------------------------------------------------------------------------------------

void GLCD_InitializePorts(void)

{

vu32 i;

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOE, ENABLE);

GPIO_StructInit(&GPIO_InitStructure);

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

GPIO_Init(KS0108_PORT, &GPIO_InitStructure);

GPIO_Write(KS0108_PORT, KS0108_CS1 | KS0108_CS2 | KS0108_CS3 | KS0108_RS | KS0108_RW | (0xFF << KS0108_D0));

}

//-------------------------------------------------------------------------------------------------

//

//-------------------------------------------------------------------------------------------------

unsigned char GLCD_ReadByteFromROMMemory(char * ptr)

{

return *(ptr);

}

//-------------------------------------------------------------------------------------------------

//

//-------------------------------------------------------------------------------------------------
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User
Posted on November 13, 2017 at 22:15

It's just GPIO manipulation. It should be easy to replace the SPL functions with their Cube/HAL counterparts.

The original author may be available to provide some support in case of problems, try to contact him.

JW