2020-08-17 08:52 AM
2020-08-17 09:10 AM
Pretty sure both SD Card slots worked out-of-the-box. Make sure nobody changed any of the jumpers or solder bridges related to the motor boards / use-case.
Not sure how well built, or complete the functionality is with demos.
STM32Cube_FW_F7_V1.16.0\Projects\STM32F769I_EVAL\Applications\FatFs\FatFs_uSD\readme.txt
I'd watch which memory was being used for DMA mode operation.
Top side microsd is the primary.
Definitely had both working on the bench here.