Skip to main content
Reema O
Associate III
August 2, 2018
Question

I am using STM32L432KC Nucleo Board. My Vref is connected to 3.3V but I wish to limit my DAC output from 0 to 1 V. How I can achieve this?

  • August 2, 2018
  • 5 replies
  • 1175 views

..

    This topic has been closed for replies.

    5 replies

    waclawek.jan
    Super User
    August 2, 2018

    Using only output values corresponding to that voltage span... ?

    JW

    Reema O
    Reema OAuthor
    Associate III
    August 2, 2018

    Yes this will be my alternative but can I used Vref Buffer for 2.5V?

    Tesla DeLorean
    Guru
    August 2, 2018

    Pretty sure the delta between VDD and VREF is constrained. The Data Sheet would be instructive on this matter.

    So truncate the values, or put an OPAMP on the output.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Reema O
    Reema OAuthor
    Associate III
    August 2, 2018

    Thanks definitely I will read datasheet for more details. Thanks to you and Jan Walclawek.

    RSonn
    Associate
    August 3, 2018

    If VDD - VREF is too constrained, use solution through hardware, a voltage divider. This will retain 12 bit resolution.​