cancel
Showing results for 
Search instead for 
Did you mean: 

I am designing an PCB with an STM32H743 and IS42S16100H 1Mx16 SDRAM. I have two issues wiring up the SDRAM as detailed below.

SPape
Associate
  1. The SDRAM has twelve address inputs A0-A11, where A11 is the bank select. In STM32CubeMX FMC section should I configure the SDRAM controller for 12 bit address and connect FMC_A0-A11 of the STM32H7 to the DRAM or configure for 11 bits and connect FMC_BA0 of the STM32H7 to A11 of the DRAM ?
  2. In the reference manual (RM0433 Rev 06, page 795) it is stated that Autoprecharge is not supported and that FMC_A(10) will always be driven low. However in sample code on the community page i noted reference to using the precharge all command which requires A10 to be high. Is the reference manual correct and if so how is the SDRAM controlled ?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0