HPDMA with UART large data transfer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-03-26 8:21 AM - last edited on 2025-03-26 8:24 AM by mƎALLEm
NUCLEO-N6 :
I was using UART to transfer a more than 100KB image to the in_buffer in the AXIRAM, so, the HAL_receive itself can not receive so much once, and I wrote a loop function it, to receive it seperately, with every timne 64KB max.
And the aligment of the data some how get wrong, do you have idea how I can use DMA of the N6 to directly transfer a more than 64KB data to the AXIRAM5 directly with only one time HALDMA beginning? the size is uint16, so max 64KB, I heard I might can use LLI of the HPDMA to do this, but I haven't learnd any thing about that, in university 64KB is far from enough, so have no experience on how to do that with LLI, do you have any documentations regarding that ?
or do you have example for receiving a 224*224*3 data through UART and DMA directly to AXIRAM with address 0x342E0000?
thanks a lot
- Labels:
-
DMA
-
STM32N6 Series
-
UART-USART