2014-07-02 5:23 AM
I am using STM32CubeMx for STM32F0x2. In ''pinout'' page, there is a checkbox called ''Activate OE'' in USB. It occupy an GPIO pin (e.g. PA15) if it is enabled.
What kind of function provided by ''Activate OE''? What is the recommended USB circuit if ''Activate OE'' is enabled?2014-07-02 7:49 AM
On the RM0091 reference manual for STM32F0, this description is found.
30.4.1 Description of USB blocksThe output enable control signal of the analog transceiver (active low) is provided externally on USB_NOE. It can be used to drive some activity LED or to provide information about the actual communication direction to some other circuitry.For ordinary USB circuit, this pin is not required. I believe an isolator of USB line is the typical application of this pin function. Tsuneo
2014-07-02 11:12 PM
Thank you