cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F042 USB - what is ''Activate OE''?

qwer.asdf
Senior
Posted on October 20, 2015 at 13:40

There is an ''Activate OE'' checkbox in STM32CubeMX is USB section of the tree which enables a ''USB_OE'' pin on PA4. I can't find any occurrence of USB_OE either in datasheet or reference manual. Can anybody tell me what is it?

Thanks.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User
Posted on October 20, 2015 at 14:03

> I can't find any occurrence of USB_OE either in datasheet or reference manual.

Maybe because it's USB_NOE... So much about Cube's consistency with the manuals.

RM0091, Ch.30.4.1:

The output enable control signal of the analog transceiver (active low) is provided externally

on USB_NOE. It can be used to drive some activity LED or to provide information about

the actual communication direction to some other circuitry.

JW

qwer.asdf
Senior
Posted on October 20, 2015 at 14:11

Thank you, Jan.