How to use program outside the main while function
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-01-31 2:41 AM
Hi there,
I am transmitting and receiving data via uart like an pl2303 bridge via USB FS. How can i manage the transmitting and receiving process outside the while so that i not block the mcu?
int main(void)
{
USB_CDC_STATUS_t check_usb;
uint16_t rx_usb;
uint16_t rx_uart;
char string_buf[RX_BUF_SIZE];
SystemInit(); // Quarz Einstellungen aktivieren
// init vom CDC
UB_USB_CDC_Init();
// init vom UART
UB_Uart_Init();
while(1)
{
// test ob USB mit PC verbunden ist
check_usb=UB_USB_CDC_GetStatus();
if(check_usb==USB_CDC_CONNECTED) {
// USB -> UART
rx_usb=UB_USB_CDC_ReceiveData(string_buf);
if(rx_usb>0) {
// wenn Daten per USB empfangen wurden
// -> alle Daten per UART senden
UB_Uart_SendData(COM3,string_buf,rx_usb);
}
// UART -> USB
rx_uart=UB_Uart_ReceiveData(COM3,string_buf);
if(rx_uart>0) {
// wenn Daten per UART empfangen wurden
// -> alle Daten per USB senden
UB_USB_CDC_SendData(string_buf,rx_uart);
}
}
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-01-31 2:46 AM
you can use some timer for x sec of time and you can have these code in the timer Interrupt service handler so that for every x time elapses the code executes.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-02-07 1:27 PM
Your current approach is called super-loop:
https://en.wikibooks.org/wiki/Embedded_Systems/Super_Loop_Architecture
It's the same used in Arduino and is the worst possible "architecture".
Better and still simple approach is to use cooperative scheduler. You can make periodic task scheduling:
But even better is event based scheduling described here:
https://embeddedgurus.com/state-space/2012/05/superloop-vs-event-driven-framework/
You can build cooperative schedulers with either or even both of these principles.
The most advanced level is using RTOS. It has real-time and other capabilities, but also requires understanding of multi-threaded programming, which is not trivial.
For beginners and also for experts with small-medium sized projects often some type of cooperative scheduler is the best choice.