2017-11-11 9:15 AM
In Cortex m3/m4, Interrupt Set Enable Registers is used to enable/disable the interrupts. How would we know which bit corresponds to which interrupt?
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0553a/Cihcajhj.html
does not give a clue on this.#interrupt-handler #stm #stm32f103 #interrupt-issue2017-11-11 12:32 PM
The NVIC interrupts are implementation specific (ie ST, ATMEL, NXP, etc), so look at the Reference Manual for the part you are using.
Review Vector Table, there is a linear application of bits and registers within the NVIC
So EXTI0 is interrupt #6
2017-11-11 2:04 PM
,
,
So this means if I want to enable hardfault and memManage Fault, which is interrupt no. 3 and 4 according to
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0553a/BABIFJFG.html
, ,I can simply do this,♯ define NVIC_ISER (*((volatile unsigned long*) 0xE000E100))
NVIC_ISER = 0x00000018, // Interrupt set enable register
Right?
2017-11-11 3:44 PM
>>Right?
No, they are SYSTEM EXCEPTIONS, not INTERRUPTS (IRQs)
The IRQs are in the NVIC, the System Exceptions are not. In the table above IRQ ♯ 0 is WWDG, IRQ ♯ 3 is RTC_WKUP
http://infocenter.arm.com/help/topic/com.arm.doc.dui0553a/Cihhjgdh.html
Use SCB->SHSCR |= (1 << 16); to enable the Memory Manager
Would suggest ORing new bits on to registers rather than assuming initial/current content