2017-03-13 04:25 AM
Hello *,
I am trying to assess feasibility of using a STM32f411 in combination with 2 4 channel class D amplifier chips (FDA4100LV) to make a USB connected surround amplifier for my computer.
I have the skills to make the USB communication and DMA buffering work. What I am uncertain about is how to use 4 i2s peripherals in sync. Each i2s peripheral seems to be outputting its own clock when configured in master mode. Is it possible to have one peripheral output the clock + 2 channel data and the 3 other peripherals output only 2 channel data on the same clock as the first i2s?
I am sorry if this question was asked before. I am dealing with quite some time pressure here and I do not have the time to do my own proper research on this matter. If someone could point me in the right direction, it would help me a lot.
Thanks, Erik.
2017-03-13 01:44 PM
Each SPI/I2S is a halfduplex unit capable of being master or slave, so yes, this should be doable, if you have a chip with 4 I2S-capable SPIs... is such among the STM32s? I have doublts the 'F411 is, I did not check.
You'll need to connect the clocks externally and watch for the GPIO matrix if this is possible at all on the package of your choice, there is quite a contention of functions on the SPI-connected pins.
Some STM32s (e.g. the original, now mid-class 'F4 line) have a crippled SPI/I2S unit marked as I2Sext which is slave-only and with internally connected SCK+WSCK to its 'master' unit. It should be possible to set both as slave, this would spare down pins and wiring, but needs to be tried. Again I don't know about the 'F411 but that's a baseline so I have doubts.
I am not sure about the connections to FDA4100V though, the public databrief hints about one clock and two data (and a rather cryptic Sinc input, which IMO might be the master clock). The I2S has TWO clocks though, plus the master clock as third, so I don't know how does this connect to that chip.
Note that in STM32 the master clock is fixed to 256* WSCK and the framing is fixed to 16- or 32-bit samples (x2 for stereo) per frame.
The SAI might be perhaps more flexible - I see TDM mentioned in that brief but I am no expert in that one.
JW
2017-03-13 02:57 PM
Ugh, looked at the 'F411 an I am much impressed, 5 SPI/I2S and the I2S2ext/I2S3ext present... not on the block diagram though (ST, do you listen?)
JW
2017-03-14 03:07 AM
I understood from the databrief that there is one Bit clock and one Word clock to the SPI and 2 data lines. I think it works like this: bit clock toggles 16 times, and on each toggle the 2 data lines are sampled, reading in the data word for Left channel 1 and Left channel 2. Then the word clock toggles and the next 16 toggles of the bit clock read in the data words for Right channel 1 and Right channel 2. This is exactly how i2s works, but with the twist that there are 2 data lines instead of one.
My question is specifically, how can I combine the data lines from multiple i2s peripherals in the stm32f411. I suspect it will be something like: Have one i2s in master mode, and the second one in slave mode and loop the clocks from master to slave somehow. Either in hardware or (preferably) in software. An alternative would be to have an external clock and put all the i2s peripherals in slave to that clock.
Does anyone know how this can be done the easiest?
2017-03-14 04:14 PM
Does anyone know how this can be done the easiest?
What do you mean by 'easiest'? There is hardly any other option than to wire up all the clocks and configure all the I2S, one to master transmitter and three to slave transmitter. As I've said above, you might use the 'crippled' I2S2ext/I2S3ext to spare down some of the wiring.
The devil is of course in the details, e.g. bandwidth considerations and particular requirements of the amplifier. I'd start with a simple I2S channel, playing back something easy like a sinewave into both channels, and feeding that into both channels of the amplifier, and evolve from that.
JW