How to unlock RDP level 1 on a STM32U0k8
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-14 3:37 PM
Hi,
I am working on a project using an STM32U031K8U6.I have been experimenting with various low power modes and somehow, It appears that I have accidentally set RDP level 1 protection.
I have been using STM32CubeIDE to create and build code and then I used Seggers J-Flash and a J-Link debugger to actually program the device. I was able to successfully program my MCU multiple times with this setup. The last time that I attempted to flash a new program I received the following error message:
---------------------------------------------------------------------------------------------------------------------------
Auto programming target (9124 bytes, 1 range) ...
- Connecting ...
- Connecting via USB to probe/ programmer device 0
- Probe/ Programmer firmware: J-Link V11 compiled Mar 14 2024 13:16:08
- Probe/ Programmer S/N: 601009238
- Device "STM32U031K8" selected.
- Target interface speed: 4000 kHz (Fixed)
- VTarget = 2.941V
- InitTarget() start
- RDP Level 1 protection is set. Reading flash memory is restricted.
- RDP Level 1 password is set.
- To unlock device please use Device Provisioner utility for STM32U0 option-bytes programming: https://wiki.segger.com/ST_STM32U0_Option_Bytes_Programming
- InitTarget() end - Took 48.5ms
- Found SW-DP with ID 0x6BA02477
- Failed to power up DAP
- InitTarget() start
- RDP Level 1 protection is set. Reading flash memory is restricted.
- RDP Level 1 password is set.
- To unlock device please use Device Provisioner utility for STM32U0 option-bytes programming: https://wiki.segger.com/ST_STM32U0_Option_Bytes_Programming
- InitTarget() end - Took 46.1ms
- Found SW-DP with ID 0x6BA02477
- Failed to power up DAP
- ERROR: Failed to connect.
Could not establish a connection to target.
- ERROR: Connect failed
- ERROR: Could not auto program target, not connected
-----------------------------------------------------------------------------------------------------------------------------
I attempted to use Seggers "Device Provisioner utility" without success. Is there some way to unlock this processor using the facilities in STM32CubeIDE or some other ST provided utility?
- Labels:
-
STM32U0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-15 1:09 AM - edited ‎2024-05-15 1:41 AM
Hello @JFP ,
Could you please try with latest release of CubeProgrammer v2.16
Then, please keep me informed about your update.
Thanks
Imen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-15 2:31 AM
Hi @JFP ,
I confirm that the regression from RDP 1 to 0 can't be done using STM32CubeProgrammer v2.16.
Our team are working to resolve this issue and will include a patch in the next version of CubeProgrammer to fix this.
Sorry, for the inconvenience it may cause and thank you for your understanding
Thanks
Imen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-15 6:49 AM
Thanks for testing this. How soon do you expect to publish the next version of STM32CubeProgrammer?