how to store signed hexadecimal data from a sensor and identify if the hex is negative or positive?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 5:23 AM
I have a sensor that can communicate via UART, I send a command and the sensor answers me with a hexadecimal frame.
I can have distance, angle, velocity values.
I know how to store the frame in a buffer but I don't know how to store it in hexa to keep the form 0xFF6F and identify if the value is negative or positive.
There is the code i have made to identifier and read value inside the buffer
extern uint8_t flag;
extern UART_HandleTypeDef huart1;
//Initialisation des commandes capteur.
uint8_t INIT[12] = {0x49, 0x4E, 0x49, 0x54, 0x04, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00}; // Init commande for the first communication and fix the Bauderate
uint8_t TDAT[12] = {0x47, 0x4E, 0x46, 0x44, 0x04, 0x00, 0x00, 0x00, 0x08, 0x00, 0x00, 0x00}; // TDAT to detect target and get the rang and the angle
uint8_t GBYE[8] = {0x49, 0x4E, 0x49, 0x54, 0x00, 0x00, 0x00, 0x00}; // commande to disconnect the sensor
void sensor_init(void){
HAL_UART_Transmit(&huart1, INIT, sizeof(INIT), 13);
HAL_Delay(75);
}
void sensor_data(void){
if (flag == 1) {
HAL_UART_Transmit(&huart1, TDAT, sizeof(TDAT), 13);
HAL_Delay(100);
flag = 0;
}
distance = k_ld7_resp[8] + k_ld7_resp[9]*0x100;
angle = (k_ld7_resp[12] + k_ld7_resp[13]*0x100) / 100;
The code for the uart callback
/*K_LD7 private variable*/
uint8_t flag = 0;
uint8_t rxByte;
char k_ld7_resp[RxBuff_SIZE];
char MainBuf_K_LD7[Main_buf_SIZE];
void Ringbuf_Reset(void){
memset(MainBuf_K_LD7, '\0', Main_buf_SIZE);
memset(k_ld7_resp, '\0', RxBuff_SIZE);
}
void HAL_UARTEx_RxEventCallback(UART_HandleTypeDef *huart, uint16_t Size){
if (huart->Instance == USART1) {
memcpy(MainBuf_K_LD7, k_ld7_resp, Size);
flag = 1;
HAL_UARTEx_ReceiveToIdle_DMA(huart, k_ld7_resp, RxBuff_SIZE);
__HAL_DMA_DISABLE_IT(&hdma_usart1_rx, DMA_IT_HT);
}
}
Solved! Go to Solution.
- Labels:
-
UART-USART
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 6:43 AM
you say something about hex but you send and rec over UART binary data.
In payload table you have info for types and conversions
simply use
int16_t angle; //stored *100 value dont use float if not required
uint16_t distance;
angle = *((int16_t *)&k_ld7_resp[12]);
distance = *((uint16_t *)&k_ld7_resp[8]);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 6:43 AM
you say something about hex but you send and rec over UART binary data.
In payload table you have info for types and conversions
simply use
int16_t angle; //stored *100 value dont use float if not required
uint16_t distance;
angle = *((int16_t *)&k_ld7_resp[12]);
distance = *((uint16_t *)&k_ld7_resp[8]);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 6:53 AM
Do not use payload bytes individually. Define a struct to receive the paylod:
typedef struct
{
uint32_t header ;
uint32_t length ;
uint16_t distance ;
int16_t speed ;
int16_t angle ;
uint16_t mag ;
} msg_t ;
msg_t data ;
If you use the data buffer to receive the sensor message, you can directly access each values.
If you have many messages types, define a struct for each message.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 6:59 AM
I tried with type int16 for the angle, now I have the negative sign but the value is completely wrong.
void sensor_data(void){
if (flag == 1) {
HAL_UART_Transmit(&huart1, TDAT, sizeof(TDAT), 13);
HAL_Delay(100);
flag = 0;
}
distance = k_ld7_resp[8] + k_ld7_resp[9]*0x100;
angle = (*(int16_t*)&k_ld7_resp[12] + (*(int16_t*)&k_ld7_resp[13])*0x100) / 100;
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 7:09 AM
Your conversion is bad dont need handle [13]*256 use my syntax and if you need angle in debree add /100. You dont show how type is angle global in your code.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 7:23 AM
Thanks, it finally works and returns the right values
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 7:26 AM
Ok if you need angle in float define as float and instead /100 add /100.0f