cancel
Showing results for 
Search instead for 
Did you mean: 

HOW TO SET UP 9 ADC DIFFERENT CHANNELS USING POLLFORCONVERSION OR DMA?

YBell.1
Associate II

Am using an Stm32f103c8 microcontroller, initially i configured 1 single ADC pin and measured temperature from the thermistor using (PollForConversion) which worked perfectly. Then I configured 5 ADC Pins to measure the temperature again and Current from 4 lithium Battery cells using (PollForConversion) but this time it doesn't work my intention is to Configure 9 ADC pins to measure single temperature, 4 channels to measure Current, and 4 channels to measure Voltage. Please someone should help me out, to get know how to use ADC Multi channels either using PollForconversion or DMA (But I don't to knew how to set up 9 ADC channels using DMA) the attached is the code that I used for 5 ADC channels using Pollforconversion but it doesn't work for me and I didn't know where was the problem. Please Help me out, thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee

Hello @YBell.1​ ,

Have a look at this example, it may help you on your project.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Use DMA

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..