2017-02-25 8:25 AM
hi
i want use sdio as 8bit mode and 48Mhz but i try to do this and i saw max 25Mhz on clk line for sdio port.
how can i set sdio as 8bit-48Mhz mode?
tnx for replay
2017-02-25 8:36 AM
You'd need to use BYPASS mode to get the Q tap clock (48 MHz nominally) as the bus clock. If you use the divider the minimum setting will be DIV2
There are timing issues with the BYPASS mode (see errata), but the SDIO clock can be up to 75 MHz, assuming you don't need it for USB, or CRYPT/HASH, which would give you 37.5 MHz safely.
Bandwidth on the SDIO is more critically limited by transfer size, small block reads/writes have significant overhead.
2017-02-25 10:07 AM
tnx for your replay.
i use this code to config sdio clock
SDIO->CLKCR = /*SDIO_CLKCR_HWFC_EN |*/ (SDIO_CLKCR_WIDBUS_0*2) | SDIO_CLKCR_PWRSAV | SDIO_CLKCR_CLKEN | (1);
i use logic analyzer to capture clk speed,with this config ,clk was around 16.6 mhz ,and if i set (0) for divide value i got around 24Mhz clk speed.
how can i disable divider?
i use usb host in my project.
2017-02-25 10:32 AM
>>
how can i disable divider?
Like I said, you'd need to use the BYPASS mode.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.