2017-02-24 8:37 AM
hello dear forum,
I copied following code from std peripheral library
however I couldnot make it work
what I am doing wrong ?
thank you
---------------
-
RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE);
----------------
NVIC_InitStructure.NVIC_IRQChannel = USB_LP_CAN1_RX0_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 5;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
--------------------------------------
CAN_Initialize(void)
{
CAN_InitTypeDef CAN_InitStructure;
CAN_FilterInitTypeDef CAN_FilterInitStructure;
/* CAN register init */
CAN_DeInit(CAN1);
CAN_StructInit(&CAN_InitStructure);
/* CAN cell init */
CAN_InitStructure.CAN_TTCM=DISABLE;
CAN_InitStructure.CAN_ABOM=DISABLE;
CAN_InitStructure.CAN_AWUM=DISABLE;
CAN_InitStructure.CAN_NART=DISABLE;
CAN_InitStructure.CAN_RFLM=DISABLE;
CAN_InitStructure.CAN_TXFP=DISABLE;
CAN_InitStructure.CAN_Mode=CAN_Mode_LoopBack;
CAN_InitStructure.CAN_SJW=CAN_SJW_1tq;
CAN_InitStructure.CAN_BS1=CAN_BS1_8tq;
CAN_InitStructure.CAN_BS2=CAN_BS2_7tq;
CAN_InitStructure.CAN_Prescaler=1;
CAN_Init(CAN1, &CAN_InitStructure);
/* CAN filter init */
CAN_FilterInitStructure.CAN_FilterNumber=1;
CAN_FilterInitStructure.CAN_FilterMode=CAN_FilterMode_IdMask;
CAN_FilterInitStructure.CAN_FilterScale=CAN_FilterScale_32bit;
CAN_FilterInitStructure.CAN_FilterIdHigh=0x0000;
CAN_FilterInitStructure.CAN_FilterIdLow=0x0000;
CAN_FilterInitStructure.CAN_FilterMaskIdHigh=0x0000;
CAN_FilterInitStructure.CAN_FilterMaskIdLow=0x0000;
CAN_FilterInitStructure.CAN_FilterFIFOAssignment=CAN_FIFO0;
CAN_FilterInitStructure.CAN_FilterActivation=ENABLE;
CAN_FilterInit(&CAN_FilterInitStructure);
/* CAN FIFO0 message pending interrupt enable */
CAN_ITConfig(CAN1, CAN_IT_FMP0, ENABLE);
return ;
}
---------------------------
void CAN_TXmit(void){
//
I call this function 10 times every second
CanTxMsg TxMessage;
/* transmit 1 message */
TxMessage.StdId=0x00;
TxMessage.ExtId=0x1234;
TxMessage.IDE=CAN_ID_EXT;
TxMessage.RTR=CAN_RTR_DATA;
TxMessage.DLC=2;
TxMessage.Data[0]=0xDE;
TxMessage.Data[1]=0xCA;
CAN_Transmit(CAN1, &TxMessage);
}
-----------------------
void USB_LP_CAN1_RX0_IRQHandler(void)
{
i++;
this variable never increase - i.e. it never enters interrupt handler
CanRxMsg RxMessage;
CAN_Receive(CAN1, CAN_FIFO0, &RxMessage);
}
#can #stm32f1032017-02-24 10:09 AM
>>
what I am doing wrong ?
I'm not interested in playing these 'guess what's wrong games', post complete and compilable code, where the context, connectivity, and intent are clearly apparent.
STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\CAN\LoopBack\main.c
Has the correct part been selected and defined for the compiler/project?
Does the IRQ handler get linked properly for the part, and match the vector table entries?
Are you using a .CPP file?
Does the chip support CAN?
Do you see an error or status returned?
Does the FIFO status indicate is has some content?
Is the problem in code you have chosen not to provide?
I've posted working examples for the F2 and F4, should be very similar, review those.
2017-02-25 6:49 AM
,
,
thanks for your kind answer Clive
I added all the CAN related code in the above post
1 ) I searched MCU forum however I find only HAL examples ,
can you provide the link to your working examples for STD library which you mentioned above
2) my CAN_Init function returns 0 which means ,
♯ define CANINITFAILED , , , , , , ,(uint8_t)0x00
is it becouse I have no physical CAN transceiver connected to the MCU ?
cannot I watch TX line with osciloscope without a tranceiver connected ?
thanks
2017-02-25 9:47 AM
In loop-back mode you shouldn't need anything on the pins.
Digging through the forum search I pulled a couple
https://community.st.com/0D70X000006SHfTSAW
https://community.st.com/0D70X000006SUMiSAO
Not familiar with your board/chip
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.