2020-01-17 10:26 PM
part number: STM32F779BI
I am using clock frequency 108 MHz ( not system clock , system clock is 216 MHZ)
I don't want to use loop
if not possible what is the maximum value i could set using timer
Solved! Go to Solution.
2020-01-20 7:44 PM
2020-01-20 8:19 PM
sorry, I had the wrong datasheet open
2020-01-20 10:37 PM
I found mistake, it works ok now
Thanks a lot
2020-01-20 10:38 PM
Thanks to all of you @Community member ,@berendi ,@turboscrew ,@Community member for your support
2020-03-02 12:20 AM
I have total 14 timers in my controller ( STM32F779BI) , I have done some timers as master-slave configration
but some timers have not master-slave configration functionality
and i know that prescaler valu maximum goes up to , i could generate maximum value of 1 millisecond
but i want to make timer of 10 milliseconds . i tried but i am getting delay of 10 ms after setting prescaler and period value
Timer clock : 108 MHz & 216 MHz , both are used for diffrent timers
how could i do that?
Dipak Garasiya
2020-03-02 12:49 AM
These are the limitations. You can slow down the APB clocks, or implement longer delays in software.
2020-03-02 10:02 AM
Cascade the timers. Make one of them tick and the other to count the first one's UGs (milliseconds), not APB-clock ticks.
Now you have a longer timer, even if in two parts.
2020-03-02 10:21 AM
Why does everything need a unique timebase?
Can't you have one, or two TIM, establish a timebase, and then count off in increments of that?
There's not going to be particularly measurable increases in power if you wake up every minute to count off 5, for example.
Normally people have a dispatch list, the timer interrupts and updates everything in the list, and whenever one task needs executing you dispatch a call. The list can be for one-off events, or repeated events with defined periodicity.
If you use a Prescaler equivalent to the MHZ of the APB the TIM can count in 1us ticks, the Period can readily allow for 1000us (1ms) or 10000us (10ms)
2020-03-02 8:59 PM
I have configured timer 6 as below, my timer clock frequency (APB1) is 108 MHz
RCC->APB1ENR |= (1<<4); // timer 6
TIM6->PSC = 108;
TIM6->EGR = TIM_EGR_UG;
TIM6->ARR = 10000;
TIM6->CR1 = TIM_CR1_CEN;
count = TIM6->CNT ;
I am not getting 10 millisecond of timer yet
2020-03-03 9:10 AM
The counters start from zero. Try PSC=107 and ARR=9999. Any closer?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.