How to send data to OP-AMP and get the value
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-05-31 8:02 AM
Posted on May 31, 2017 at 17:02
Hello,
I'm still trying to continue the programmation of my STM32F405 board and I have (again) a little problem. I use a OP-AMP to compare 2 signals by sending him a integer. The return value is always the same even if I change the initial integer and I dont understand why...I hope this is understandable.
Can you explain me what's wrong in my code or eventually show me some documentation ?void gpio_initialize(){ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); GPIO_InitTypeDef GPIO_initStruct_PA_an2; GPIO_initStruct_PA_an2.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5; GPIO_initStruct_PA_an2.GPIO_Mode = GPIO_Mode_AN; GPIO_initStruct_PA_an2.GPIO_OType = GPIO_OType_PP; GPIO_initStruct_PA_an2.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_initStruct_PA_an2.GPIO_Speed = GPIO_Speed_100MHz; GPIO_Init(GPIOA, &GPIO_initStruct_PA_an2);}void dac_initialize(){ DAC_InitTypeDef DAC_InitStructure; RCC_APB1PeriphClockCmd(RCC_APB1Periph_DAC, ENABLE); DAC_InitStructure.DAC_Trigger = DAC_Trigger_Software; DAC_InitStructure.DAC_WaveGeneration = DAC_WaveGeneration_None;// DAC_WaveGeneration_Triangle; DAC_InitStructure.DAC_OutputBuffer = DAC_OutputBuffer_Enable; //DAC_InitStructure.DAC_LFSRUnmask_TriangleAmplitude = DAC_TriangleAmplitude_4095; DAC_Init(DAC_Channel_1, &DAC_InitStructure); DAC_Init(DAC_Channel_2, &DAC_InitStructure); DAC_Cmd(DAC_Channel_1, ENABLE); DAC_Cmd(DAC_Channel_2, ENABLE); DAC_SoftwareTriggerCmd(DAC_Channel_1, ENABLE); DAC_SoftwareTriggerCmd(DAC_Channel_2, ENABLE);}void adc_initialize(){ ADC_InitTypeDef ADC_init_struct12b; //Clock configuration RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE); //ADC structure configuration ADC_DeInit(); ADC_init_struct12b.ADC_DataAlign = ADC_DataAlign_Right; ADC_init_struct12b.ADC_Resolution = ADC_Resolution_12b; ADC_init_struct12b.ADC_ContinuousConvMode = ENABLE; ADC_init_struct12b.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1; ADC_init_struct12b.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_init_struct12b.ADC_NbrOfConversion = 1; ADC_init_struct12b.ADC_ScanConvMode = DISABLE; ADC_Init(ADC1, &ADC_init_struct12b);//Initialize ADC with the previous configuration ADC_RegularChannelConfig(ADC1, ADC_Channel_1, 1, ADC_SampleTime_3Cycles); ADC_Cmd(ADC1, ENABLE);}int adc_convert_sence(){ ADC_SoftwareStartConv(ADC1); while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC)); return ADC_GetConversionValue(ADC1);}int main(void){ gpio_initialize(); adc_initialize(); dac_initialize(); systickInit(1000); DAC_SetChannel2Data(DAC_Align_12b_R, 2048); while (1) { DAC_SetChannel1Data(DAC_Align_12b_R, 0); delay_ms(20); resultSence = adc_convert_sence(); printf('%d / ', resultSence); DAC_SetChannel1Data(DAC_Align_12b_R, 10); delay_ms(20); resultSence = adc_convert_sence(); printf('%d / ', resultSence); DAC_SetChannel1Data(DAC_Align_12b_R, 500); delay_ms(20); resultSence = adc_convert_sence(); printf('%d / ', resultSence); }}Thanking you in advance,
Nicolas-
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-06-02 3:55 AM
Posted on June 02, 2017 at 12:55
1 check DAC output with a digi-meter.
2 try to config the op amp as a buffer first, and check if you can read back the dac value.
3 check integrator RC constant to see whether it would be saturated after 20 msec.