2025-07-15 8:18 AM
i whant to know if the B-CAMS-OMV is compatible with the 32F746GDISCOVERY, NUCLEO-N657X0-Q, and the STM32N6570-DK?
because i why didn't I find the specific connector data of the 3 kits regarding the camera,
And I want to know this one camera B-CAMS-OMV is good for me for the 3 different kits?
Solved! Go to Solution.
2025-07-28 6:31 PM
B-CAMS-IMS (at B-CAMS-IMX - Camera module bundle for STM32 boards - STMicroelectronics) should be supported by N6 Nucleo and DK. thanks!
2025-07-21 11:32 PM
Both NUCLEO-N657X0-Q and the STM32N6570-DK supports camera module with CSI interface, so they are not compatible with B-CAMS-OMV which is designed to support DCMI interface.
Based on 32F746GDISCOVERY schematic, B-CAMS-OMV should work with this board.
2025-07-28 1:46 PM
okey , i need a MIPI CSI-2 camera!...
2025-07-28 6:31 PM
B-CAMS-IMS (at B-CAMS-IMX - Camera module bundle for STM32 boards - STMicroelectronics) should be supported by N6 Nucleo and DK. thanks!