How to remap CAN-Pins for a STM32F042 TSSOP20 Chip
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-01 12:45 PM
Hi,
I'm going to use a STM32F042F6P in TSSOP20 - case for a application using CAN - connectivity. The low-pin-version of the STM32F042 demand to remap the CAN-pins to alternate pins.
I already discovered the hint for bit 4 (PA11_PA12_RMP) of SYSCFG_CFGR1 for repmapping PA11/PA12 to PA9/PA10 (pin 17/18 of the TSSOP20 chip), but unfortunately it simply doesn't work.
I checked my firmware with a LQFP32 type of the chip (NUCLEO-Board) with CAN - pins on PA11/PA12 - so everything seams to work properly. My idea was simply to change SYSCFG_CFGR1.4 - bit for the smaller case chip and have fun with the stuff.
Please can anybody tell me weather there is anything else to do transfer my CAN-Program from STM32F042K4U (LQFP32) to STM32F042F6P (TSSOP20), or is the remap-bit the only neccessary changing?
My second question is, does pin-remapping work with GPIOs to? As a test, I tried to remap PA11/PA12 to PA9/PA10 and to toggle PA11/PA12 then, but this didn't run too.
Thanks a lot for your help.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-01 1:22 PM
Don't you need to do the PA11/PA12 vs PA9/PA10 switch, and then set the AF4 for PA11/PA12 pin configuration?
https://www.st.com/resource/en/datasheet/stm32f042f6.pdf
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-01 1:38 PM
/* Enable GPIO TX/RX clock */
__HAL_RCC_SYSCFG_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_REMAP_PIN_ENABLE(HAL_REMAP_PA11_PA12); // SYSCFG_CFGR1_PA11_PA12_RMP
/* Enable CAN clock */
__HAL_RCC_CAN1_CLK_ENABLE();
/*##-2- Configure peripheral GPIO ##########################################*/
/* UART TX GPIO pin configuration */
GPIO_InitStruct.Pin = GPIO_PIN_11 | GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF4_CAN;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
...
sourcer32@gmail.com
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-01 1:56 PM
Hello Clive,
thank you very much for your prompt reply.
I use the MIKROE C compiler, and they offer a routine for CAN - Setup including bit timing, pin setup etc. There AF4 configuration is done. With the LQFP - type it worked well.
But do you know whether one step is to be done before the other, or is that not important?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-02 10:43 PM
Hi there,
Did you notice that Clive's example first enabled the clock for the SYSCFG ? Are you also enabling the clock for SYSCFG before changing bit 4 in SYSCFG_CFGR1 ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-03 10:33 PM
Good morning Clive and Kraal,
thank you very much for your help again.
With your advice I was able to fix the problem.
I myself would never have come up with the idea of searching this corner for the cause of the error.
You were therefore a great help - thank you again.