2024-05-07 08:39 AM - edited 2024-05-14 11:54 PM
Hi,
As the title described, how to mitigate the current behavior when stm32 is applied power? My commercial power system are quite sensitive when MCU is power on.
For example, let stm32 enters into low power mode once power is on and then control the chip enter into fromal user mode. Would that help?
thanks.
2024-05-17 05:59 AM
Sigh. The rise of the "Arduino Generation" that just "hooks stuff up". We're all doomed.
2024-05-18 01:11 AM
We do want to help. Having re-read this thread, I still don't know how often the trip happens - if at all. At some stage you'll have to do something that can't be undone.
I'll say I don't have a current probe. I always regarded them as too expensive given how infrequently I would use them, and the different insight from the voltages either side of a series-resistor can sometimes be helpful.