How to properly connect the X-Nucleo-LPM01A to a nucleo-L152RE (GPIO not working)
Hello!
I'm trying to power only the mcu on a nucleo-L152RE dev-kit from the X-nucleo-LPM01A to measure it's power consumption, however i suspect the mcu is not running, and debugging it provides wierd results that I cant make sense of.
The program I'm trying to run is as simple as it gets: the onboard LED toggles on and off with a delay of 3000 ms. When powering the board from USB (debugger & mcu powered), everything works fine.
The issue arise when I try to disable the debugger and only power the mcu from the X-nucleo. I do this by connecting CN14 pin 1 (GND) and CN14 pin 3 (VOUT (+)) on the X-nucleo to GND and VDD (pin on JP6, IDD) on the dev-kit, respectively.
In this configuration, the x-nucleo report a current draw of about 1mA, however the LED is not blinking.
I've followed the exact steps in the community post explaining this ("How to connect my stm32 to the x-nucleo-lpm01a"), read the user manual for the X-nucleo (UM2243) and nucleo-L152RE (UM1724) thoroughly, inspected the schematics (C-04 version, MB1136) and read other sources i found, to no avail.
Here are a few comments about what I've tried, and the results I got:
- Powering the dev-kit from USB with JP5 (U5V/E5V selection) and JP6 (IDD) removed, the mcu still runs, and the LED is blinking, although dimmer. This is what confuse me the most. According to schematics, this should leave +3v3 and VDD at 0V, but I read around +1.9V.
- I've tried with JP5 on and off - no difference.
- I've tried removing SB12 (NRST from mcu to debugger) and SB2 (3v3 reg output to JP6, IDD) and powered through +3V3 pin instead (JP6, IDD connected). This is specified in the UM1724 dev-kit manual, but it makes no difference - the LED is still not working.
I feel like I've tried anything at this point, but it's still not working. Can anyone help me understand why this isn't working?