How to pass a variable read in an interruption to main()
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-14 06:14 AM
I'm reading a serial ADC from an interruption (24 bits)
I need to pass its read value to the main()
I have defined in /* USER CODE BEGIN PV */ a volatile variable uint32_t xxxxx
The xxxxx variable is right inside the interruption routine but it becomes 0x01FFFFFE when called in main()
How can I pass the xxxxx variable from void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) to main()?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-14 06:18 AM
A global variable should be visible in main()
You might want another flag to indicate the presence of new data if that can't be inferred from the data itself.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-14 09:27 AM
I did as it follows
/* USER CODE BEGIN PV */
uint32_t show;volatile uint32_t measure;/* USER CODE END PV */int main(void) {
HAL_Init();
SystemClock_Config(); MX_GPIO_Init(); while (1) { show = measure; }}void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{ uint8_t i; if(GPIO_Pin== GPIO_PIN_3) { HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET); measure = 0; for (i=0; i<24;i++) { HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_SET); if (HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_3)) { measure ++; } measure = measure*2; HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET); } HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_SET);} else{
__NOP(); } }show and measure declared as global
measure is valid in the void
HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) scope
but become 0x1FFFFFE in main () when show = measure
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-14 09:55 AM
Probably because you're causing PA3 to bang up and down in an interrupt that triggers on PA3?
Consider using a flag to indicate if it filled the variable, or queuing the measurements, so you can see if the routine has entered multiple times.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-14 10:17 AM
I have added a new global variable variable iterac
uint8_t iterac;
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{ uint8_t i; if(GPIO_Pin== GPIO_PIN_3) { newData = 1; HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET);measure
= 0; for (i=0; i<24;i++) { HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_SET); if (HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_3)) {measure ++; }measure
=measure
*2; HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET); } HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_SET); } else{ __NOP(); } iterac = i;}debugging (breakpoint at iterac = i) I see that the callback always return when iteract = 24 (that is i=24)
and measure is 0x0100033E
after 24 pulses at PA6, PA3 has been 0x0100033E. That is, there have been edges at PA3 but the interruption has only executed once.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-14 11:02 AM
>>
I see that the callback always return when iteract = 24 (that is i=24)
Well no doubt, I'm suggesting that the interrupt is reentering, not preemptively.
Make iteract a 32-bit free running counter, ie don't reset it to zero at each interrupt entry, or to the loop count.
In your main loop printf() iteract and show/measure to the SWV console.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-14 11:08 AM
Why the heck is everything being moderated today?
volatile uint32_t iterac = 0;
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{uint8_t i;iterac++; // Entry count
if(GPIO_Pin== GPIO_PIN_3) {
newData = 1;HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET);measure
= 0;for (i=0; i<24;i++){HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_SET);if (HAL_GPIO_ReadPin(GPIOA, GPIO_PIN_3)){measure ++;}measure
=measure
*2;HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET);}HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_SET);} else{__NOP();}}...
while (1) {
if (measure != 0xFFFFFFFF)
{
show = measure;
measure = 0xFFFFFFFF;
printf('%08X %08X\n', iterac, show);
}
}
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-14 11:21 AM
iterac continously increasing
show and measure 0x01FFFFFE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-14 11:59 AM
And that's not what you see when you break-point the exit of the IRQ? Don't single step the clocking
Using what tools? Or what processor/board?
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-15 01:42 AM
I'm configuring the board by means STM32CubeMX
The processor is the STM32L100RC
The board is designed by me
I'm going to review the hardware. Perhaps a noise glitch in the EXTI/DataIN (PA3) is triggering the interrupt