cancel
Showing results for 
Search instead for 
Did you mean: 

Cancel a pending UART recieve

John Craven
Senior
Posted on January 16, 2017 at 23:02

If i start an UART receive with an interrupt looking for the next inbound byte/char;

HAL_UART_Receive_IT(&huart1, &UART1_Data, 1);

how can i cancel the receive before receiving the next byte/char?

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Posted on January 16, 2017 at 23:08

I'd imagine you could flag it yourself and handle in the callback.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on January 16, 2017 at 23:13

when you say flag it, do you mean force an interrupt by setting a interrupt bit in the uart and then handling the interrupt?

T J
Lead
Posted on January 17, 2017 at 00:29

did you fix it ?

would you like to use the DAM rx functions ?

I get an interrupt on each and every character.

Posted on January 17, 2017 at 02:57

I mean on your side, presumably you're going to want it to receive again at some point, and if you don't keep servicing it you'll have it overrun.

Flag that you want to cancel, eat the byte if you don't want it, and don't light off another.

Why are you looking to cancel it? Do you have some secondary buffering, or are you using this method to pull and process data a byte at a time.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
John Craven
Senior
Posted on June 15, 2017 at 17:29

Updating this thread. My original post and other similar posts have been heard by the HAL developers.

New HAL functions were added recently for UARTs including;

/* Transfer Abort functions */

HAL_StatusTypeDef HAL_UART_Abort(UART_HandleTypeDef *huart);

HAL_StatusTypeDef HAL_UART_AbortTransmit(UART_HandleTypeDef *huart);

HAL_StatusTypeDef HAL_UART_AbortReceive(UART_HandleTypeDef *huart);

HAL_StatusTypeDef HAL_UART_Abort_IT(UART_HandleTypeDef *huart);

HAL_StatusTypeDef HAL_UART_AbortTransmit_IT(UART_HandleTypeDef *huart);

HAL_StatusTypeDef HAL_UART_AbortReceive_IT(UART_HandleTypeDef *huart);

as of the time of this update, not all HAL series have been updated, but will be as each new series FW is released.

I will test HAL_UART_AbortReceive_IT(UART_HandleTypeDef *huart) in my original project shortly.