2021-08-12 09:52 PM
Hello,
I would send the packet between a client and a server with over 20 bytes.
I have searched all communities and haven't fount out any actual solution. (Such as, doing 'aci_gatt_exchange_config()' function or exchange ATT_MTU value)
Is it possible to increase the maximum size of any packet sent between a client and a server?
Thanks,
2024-12-03 02:21 AM