2018-02-13 1:22 PM
Hello everyone,
I try to develop a Bluetooth interface with a X-NUCLEO-IDB05A1. In this case, I want to firstly test the SensorDemo from 'CUBE-BLE1' package. I open the project with System Workbench but unfortunatelly after the first success build, I get errors in all my .c files. The errors are like 'Type 'xxx' could not be resolved'.
I ask myself to see if it isn't a problem caused by the path files length. So, I have tried to create a new project and import manually all files but with no succes ...
Anyone have a solution or a step that I could miss ?Kinds regard,Sylvain.
#x-nucleo-idb05a1 #x-cube-ble1 #sensordemo