How to implement SPR PPS Mode for the STM32F072 ?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-11-17 2:45 PM
Hi,
I am using an NUCLEO-F072RB Board with an STUSB1602 Type-C Controller Expansion Board.
My Goal is to program a Sink application which is able to use the PPS Mode. Furthermore I am using the STM32_MB1303_SNK_ONLY Project as a reference.
My Questions are as follows:
- Is it possible ?
- What would I have to do in order to implement it. I know how to read the PDOs from the Source but not the APDOs which are needed for the PPS mode.
Your help and feedback is highly appreciated.
Kind regards
Shinji
Labels:
- Labels:
-
STM32F0 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0