cancel
Showing results for 
Search instead for 
Did you mean: 

How to implement IAP(Ymodem Protocol) on DualCore(h745)?

yolominwoo
Associate III

I'm tring implement IAP on NUCLEO-H745ZI-Q.

So. I seen STM32h743-eval IAP Example.

But I have two bank and two core for cm7 and cm4.

I don't know how to implement the bootloader.

And should I create and transfer bin files for cm4 and cm7 respectively?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

You can merge the hex files (see this thread) and do the operation once as stated previously, the two cores are seeing the same memory.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5

Up to you..

Both cores see the same memory. 

You could use two binaries or put some kind of object or meta data, to describe multiple sections with lengths and addresses.

You could also stage the update in a QSPI

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

When i implement IAP, then make bin then Make each bin files for CM4, CM7.

Download twice for cm4 and cm7 or merge bin and once download?

You'll need to make that choice. If you do a single download you must impart how the content is split up.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

You can merge the hex files (see this thread) and do the operation once as stated previously, the two cores are seeing the same memory.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thanks I'm try it.