cancel
Showing results for 
Search instead for 
Did you mean: 

How to fix '' invalid project path: include path no found'' using SW4STM32

Manel Asgarzadeh
Associate II
Posted on May 08, 2018 at 20:46

Hi there,

i imported an existing project into my project explorer using SW4STM32 and when i built the project i got a warning saying : ' invalid project path: include path no found'

ps: am using eclipse Version: Neon.3 Release (4.6.3)

is there anyone would can help me ?

thanks in advance

kind regards
5 REPLIES 5
Imen.D
ST Employee
Posted on May 18, 2018 at 13:42

Hello,

Check that the Include Paths are properly configured into your project from the correct directories. 

Properties > C/C++ Generals > Paths and Symbols > Includes tab.

With Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on May 18, 2018 at 14:00

Hello,

Actually I don’t know if it is

This is my path : c:/stm32workbench/NZ32-sc151_Template-master/SW4STM32

but I don’t find it in the include tab

Here is what I get :

Kind regards

On Fri, May 18, 2018 at 4:13 PM Imen D <st-microelectronics@jiveon.com>

________________

Attachments :

image_123986672.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hxbk&d=%2Fa%2F0X0000000b0A%2FtKcuNuGyqz.jjhY._1uZDA3bCQ0KXENH0LhJF3PTIJk&asPdf=false
henry.dick
Senior II
Posted on May 22, 2018 at 13:03

It is trying to tell you that the path specified in the project properties section is not valid. Likely it doesn't exist, or is not updated . 

Posted on May 22, 2018 at 11:56

Hello

manel

,

Can you please share your project and .log (under yourworkspace/.metada/.log) for more check.

With Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on May 22, 2018 at 13:05

Hi , yeah well I got that but what I want to know is how to fix it

Regards.

On Tue, May 22, 2018 at 3:34 PM dhenry <st-microelectronics@jiveon.com>