2013-12-10 11:02 PM
hello :
I buy the STM32F40G-JAVA eval board,i got a problem when i used the MricoEJ to develop the project. I read the STM32Java-UI-PACK user's Manual,In the 7.2.4 it shows that how to edit stroyboard, i did it follow the document said ,however, i don't know how to execute it and display it in the simJPF you know, i write it like this,,i read the class summary about stroyBoard ,it show that it have the method ,then i write the code ,In a pity ,it has error,can't find the source,i don't know why.public class MyTest { /** * @param args */ public static void main(String[] args) { // TODO Auto-generated method stub Display display; display=Display.getDefaultDisplay(); StoryBoard.loadStory(''Mystoryboard'').run(display); }}2013-12-11 08:46 AM
Hi Roy,
Some ideas: * Don't forget to Enable storyboard support in your project: launcher In menu Run configurations JPF Configuration Storyboard Enable story board spport and add you storyboard file . * Other ideas: Try the story board example proposed in File Java example. The code is somethning like that:import
com.is2t.storyboard.StoryBoard;
import
ej.microui.io.Display;
public
class
StoryboardAppnotesLauncher {
public
static
void
main(String[] args) {
// 1. load
storyboard
fromImmutables
StoryBoard myboard = StoryBoard.loadStory(
''Example''
);Display[] displays = Display.getAllDisplays();
// 2. run it on last available display
myboard.run(displays[displays.
length
- 1]);}
} Best regards Phil
2013-12-17 06:24 AM
hello phil:
thanks so much. i figure out the problems. can i have your email or skype , can we be a friend, you can add my skype , my email: aizhixi@gmail.com my skype: aizhixi106 roy.huIn the end ,thanks so much.