2015-01-06 5:03 AM
I use STM429 and 128Mb SDRAM and want to decare a big array in keil. How to declare it? How to let keil linker know the array is in external RAM?
I defines uint8_t temp[1024*1024], but linker error L6406E: no space in execution region. Thanks.2015-01-06 5:22 AM
I defines uint8_t temp[1024*1024], but linker error L6406E: no space in execution region.
Thanks. uint8_t *temp = (uint8_t *)0xa0000000 Or learn about section attributes in C and section definitions in the linker.2015-01-06 6:02 AM
char buf[256] __attribute__ ((section(''.sdram'')));
Then you'd need to describe the memory regions and sections in the scatter file, and make sure you initialize the SDRAM in SystemInit() so it's functional prior to the C run time code initializing the statics.
This uses the CCM memory, but is on point, add a RAM1 section for the external SDRAM
[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Usage%20of%20CCM%20Data%20RAM%20in%20KEIL&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx?Paged%3DTRUE%26p_StickyPost%3D%26p_DiscussionLastUpdated%3D20140926%252010%253a32%253a21%26p_ID%3D43964%26View%3D%257bF47A9ED8%252dE726%252d42BE%252dACED%252d732F13B66581%257d%26FolderCTID%3D0x012001%26PageFirstRow%3D41¤tviews=32]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Usage%20of%20CCM%20Data%20RAM%20in%20KEIL&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx?Paged%3DTRUE%26p_StickyPost%3D%26p_DiscussionLastUpdated%3D20140926%252010%253a32%253a21%26p_ID%3D43964%26View%3D%257bF47A9ED8%252dE726%252d42BE%252dACED%252d732F13B66581%257d%26FolderCTID%3D0x012001%26PageFirstRow%3D41¤tviews=32
2015-01-07 5:55 AM