2021-10-14 5:38 AM
I need to request constant data packets using DMA via SPI on master (STM32H745ZI) from slave(iNemo-M1 with STM32F103REY6 MCU).
Despite I have problem using DMA on master side for while I can using blocking receiving.
Main problem is with slave side.
If I sending from slave to master using HAL_SPI_Transmit, HAL_SPI_TransmitReceive or in loop with LL_SPI_TransmitData16 all working correcly and master receiving data.
If I'm using DMA transfer using LL DMA's TC interrupt occurs but DR register never filled and I see on master only 00s.
Here SPI1 initialization generated in CubeIDE (MCU package 1.8.4):
void MX_SPI1_Init(void)
{
/* USER CODE BEGIN SPI1_Init 0 */
/* USER CODE END SPI1_Init 0 */
LL_SPI_InitTypeDef SPI_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
/* Peripheral clock enable */
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SPI1);
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_GPIOA);
/**SPI1 GPIO Configuration
PA5 ------> SPI1_SCK
PA7 ------> SPI1_MOSI
PA6 ------> SPI1_MISO
PA4 ------> SPI1_NSS
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_5|LL_GPIO_PIN_7|LL_GPIO_PIN_4;
GPIO_InitStruct.Mode = LL_GPIO_MODE_FLOATING;
LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_6;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* SPI1 DMA Init */
/* SPI1_TX Init */
LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_3, LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
LL_DMA_SetChannelPriorityLevel(DMA1, LL_DMA_CHANNEL_3, LL_DMA_PRIORITY_LOW);
LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_3, LL_DMA_MODE_NORMAL);
LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_CHANNEL_3, LL_DMA_PERIPH_NOINCREMENT);
LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_CHANNEL_3, LL_DMA_MEMORY_INCREMENT);
LL_DMA_SetPeriphSize(DMA1, LL_DMA_CHANNEL_3, LL_DMA_PDATAALIGN_HALFWORD);
LL_DMA_SetMemorySize(DMA1, LL_DMA_CHANNEL_3, LL_DMA_MDATAALIGN_HALFWORD);
/* SPI1_RX Init */
LL_DMA_SetDataTransferDirection(DMA1, LL_DMA_CHANNEL_2, LL_DMA_DIRECTION_PERIPH_TO_MEMORY);
LL_DMA_SetChannelPriorityLevel(DMA1, LL_DMA_CHANNEL_2, LL_DMA_PRIORITY_LOW);
LL_DMA_SetMode(DMA1, LL_DMA_CHANNEL_2, LL_DMA_MODE_NORMAL);
LL_DMA_SetPeriphIncMode(DMA1, LL_DMA_CHANNEL_2, LL_DMA_PERIPH_NOINCREMENT);
LL_DMA_SetMemoryIncMode(DMA1, LL_DMA_CHANNEL_2, LL_DMA_MEMORY_INCREMENT);
LL_DMA_SetPeriphSize(DMA1, LL_DMA_CHANNEL_2, LL_DMA_PDATAALIGN_HALFWORD);
LL_DMA_SetMemorySize(DMA1, LL_DMA_CHANNEL_2, LL_DMA_MDATAALIGN_HALFWORD);
/* USER CODE BEGIN SPI1_Init 1 */
/* USER CODE END SPI1_Init 1 */
SPI_InitStruct.TransferDirection = LL_SPI_FULL_DUPLEX;
SPI_InitStruct.Mode = LL_SPI_MODE_SLAVE;
SPI_InitStruct.DataWidth = LL_SPI_DATAWIDTH_16BIT;
SPI_InitStruct.ClockPolarity = LL_SPI_POLARITY_LOW;
SPI_InitStruct.ClockPhase = LL_SPI_PHASE_1EDGE;
SPI_InitStruct.NSS = LL_SPI_NSS_HARD_INPUT;
SPI_InitStruct.BaudRate = LL_SPI_BAUDRATEPRESCALER_DIV8;
SPI_InitStruct.BitOrder = LL_SPI_MSB_FIRST;
SPI_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE;
SPI_InitStruct.CRCPoly = 10;
LL_SPI_Init(SPI1, &SPI_InitStruct);
/* USER CODE BEGIN SPI1_Init 2 */
/* USER CODE END SPI1_Init 2 */
}In main.c I'm setup DMA as follows:
void initSlaveSpi()
{
LL_DMA_DisableChannel(DMA1, LL_DMA_CHANNEL_2);
LL_DMA_DisableChannel(DMA1, LL_DMA_CHANNEL_3);
LL_DMA_ClearFlag_TC2(DMA1);
LL_DMA_ClearFlag_TC3(DMA1);
LL_DMA_ClearFlag_TE2(DMA1);
LL_DMA_ClearFlag_TE3(DMA1);
LL_SPI_EnableDMAReq_TX(SPI1);
LL_SPI_EnableDMAReq_RX(SPI1);
LL_DMA_EnableIT_TC(DMA1, LL_DMA_CHANNEL_2);
LL_DMA_EnableIT_TE(DMA1, LL_DMA_CHANNEL_2);
LL_DMA_EnableIT_TC(DMA1, LL_DMA_CHANNEL_3);
LL_DMA_EnableIT_TE(DMA1, LL_DMA_CHANNEL_3);
LL_SPI_Enable(SPI1);
}DMA channel 3 used to transmitting data.
Each DMA transfer begins when I call following function:
void startSpiDmaTransfer()
{
LL_DMA_DisableChannel(DMA1, LL_DMA_CHANNEL_2);
LL_DMA_DisableChannel(DMA1, LL_DMA_CHANNEL_3);
LL_DMA_SetDataLength(DMA1, LL_DMA_CHANNEL_2, 2);
LL_DMA_SetDataLength(DMA1, LL_DMA_CHANNEL_3, 2);
LL_DMA_ConfigAddresses(DMA1, LL_DMA_CHANNEL_3, (uint32_t)&txBuf,
(uint32_t)&SPI1->DR,
LL_DMA_DIRECTION_MEMORY_TO_PERIPH);
LL_DMA_ConfigAddresses(DMA1, LL_DMA_CHANNEL_2, LL_SPI_DMA_GetRegAddr(SPI1), (uint32_t)rxBuf,
LL_DMA_DIRECTION_PERIPH_TO_MEMORY);
LL_SPI_EnableDMAReq_TX(SPI1);
LL_SPI_EnableDMAReq_RX(SPI1);
LL_DMA_ClearFlag_TC2(DMA1);
LL_DMA_ClearFlag_TC3(DMA1);
LL_DMA_ClearFlag_TE2(DMA1);
LL_DMA_ClearFlag_TE3(DMA1);
LL_DMA_EnableChannel(DMA1, LL_DMA_CHANNEL_3);
LL_DMA_EnableChannel(DMA1, LL_DMA_CHANNEL_2);
}DMA transfer complete interrupt looks very simple:
void spiTxTransferComplete()
{
LL_DMA_ClearFlag_TC3(DMA1);
txFinished = 1;
}Where txFinished is flag I'm checking before starting next DMA transfer.