2012-07-10 7:09 AM
According to the attached. I do not understand how to set the clock correctly TIMER From what I understand, TIMXCLK PCLK1 = 2 * and 2 * = TIM1CLK PCLK2 But not found in the manual or the information in the datasheet. Can anyone help me?
void vConfigura_RCC(void)
{ RCC_DeInit(); // Deinitialize RCC RCC_HSEConfig(RCC_HSE_ON); // Enable HSE (external crystal) HSEStartUpStatus = RCC_WaitForHSEStartUp(); // Wait till HSE is ready if (HSEStartUpStatus == SUCCESS) { FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable); // Enable Prefetch Buffer FLASH_SetLatency(FLASH_Latency_2); // Flash 2 wait state RCC_HCLKConfig(RCC_SYSCLK_Div1); // HCLK = SYSCLK = 72Mhz RCC_ADCCLKConfig(RCC_PCLK2_Div6); // ADCCLK = PCLK2/6 = 12MHz RCC_PCLK2Config(RCC_HCLK_Div1); // PCLK2 = HCLK = 72Mhz RCC_PCLK1Config(RCC_HCLK_Div2); // PCLK1 = HCLK / 2 = 36Mhz RCC_PLLConfig(RCC_PLLSource_HSE_Div1, RCC_PLLMul_9); // PLLCLK = 8Mhz x 9 = 72Mhz RCC_PLLCmd(ENABLE); // Enable PLL while (RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET); // Wait till PLL is ready RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); // Select PLL as system clock source while (RCC_GetSYSCLKSource() != 0x08); // Wait till PLL is used as system clock source }/* PCLK1 = HCLK/4 */
RCC_PCLK1Config(RCC_HCLK_Div8); // Ajusta CLOCK dos Perifericos de APB1 RCC_PCLK2Config(RCC_HCLK_Div8); // Ajusta CLOCK dos Perifericos de APB2 /* TIM3 clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE); /* GPIOA and GPIOC clock enable */ RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO, ENABLE); } #timer-clock-rcc2012-07-10 7:26 AM
You need to look at the RCC Clock Tree in the REFERENCE MANUAL, See Pg 123 ''Figure 11 Clock Tree''
The timers here both look to be clocked at 18 MHz.2012-07-10 7:57 AM
THANKS Clive1
If prescaler not set=1, then prescaler=2;2012-07-10 8:17 AM
It's really to let the timers run at 72 MHz (logic rated at this speed) when the bus is at 36 MHz, but you can't exceed the input clock. Basically you lose a divider, rather than have a multiplier.
Where HCLK = 72 MHz RCC_HCLK_Div1, TIMCLK 72 MHz RCC_HCLK_Div2, TIMCLK 72 MHz RCC_HCLK_Div4, TIMCLK 36 MHz RCC_HCLK_Div8, TIMCLK 18 MHz The part always generates the slower clocks in the divider chain, the prescaler just picks which one to gate out (tap) to down stream logic.2012-07-10 9:38 AM
Let me see if I understood...
Here the HCLK was configured with the same frequency of the SYSCLK=72MHz
RCC_HCLKConfig(RCC_SYSCLK_Div1);// HCLK = SYSCLK = 72Mhz
Here, The Clock of APB1 and APB2 was configures of HCLK/4=18MHz
RCC_PCLK1Config(RCC_HCLK_Div4);// Ajusta CLOCK dos Perifericos de APB1
RCC_PCLK2Config(RCC_HCLK_Div4);// Ajusta CLOCK dos Perifericos de APB2
I can Configure with RCC_HCLK_Div1, Div2, Div3 or Div4 like you show on table
In this case the TIM1CLK and TIMXCLK =36MHz, because:
TIMXCLK=RCC_PCLK1Config*2;
TIM1CLK=RCC_PCLK2Config*2;on the page 123 (REFERENCE_MANUAL)
Only if the RCC_PCLK(X)Config=1
TIMXCLK=RCC_PCLK1Config*1;
TIM1CLK=RCC_PCLK2Config*1;on the page 123 (REFERENCE_MANUAL)
THANKS again Clive1