2020-10-06 12:35 AM
Hello, for decreasing the power coonsumption I want to change HSI to LSI. This is the HSI clock configurations for 72 Mhz:
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_ADC|RCC_PERIPHCLK_USB;
PeriphClkInit.AdcClockSelection = RCC_ADCPCLK2_DIV6;
PeriphClkInit.UsbClockSelection = RCC_USBCLKSOURCE_PLL_DIV1_5;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
}
And I want to enable LSI then disable the HSI as follows:
//Turn on the LSI
RCC->CSR|=RCC_CSR_LSION;
//Turn off the HSI
RCC->CR&=~(RCC_CR_HSION);
Is it a correct way to change the system clock to 40 kHz? Or do I any others things that must be done? Any I am not sure from the order. Should I first disable HSI then turn on the LSI or should I first turn on the LSI then turn off the HSI?
2020-10-06 12:45 AM
Which STM32? Not all models allow to use LSI as system clock.
Generally, you
Meantime, you might want to change settings of those peripherals which are clock-dependent, e.g. UART baudrate.
Read the RCC chapter in RM.
JW
2020-10-06 12:48 AM
Thank you, that is STM32F10x
2020-10-06 1:10 AM
Yes it does not let LSI being used as the system clock, unfortunately.
2020-10-06 1:06 PM
You must also care for wait states and maybe other settings, like voltage regulators.