2013-12-19 06:03 AM
Hello everybody,
I communicate with a popular screen, the DOGM128 (ST7565RLCD Controller) with my STM32F4 uC. Sometimes, when I power on my board, the screen have troubles to be initialized (it remains white, whatever I do). I think it's due to the SPI speed, that I can't estimate. The max SPI clock speed of the screen controller is 20MHz. This is my SPI screen init :RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
GPIO_InitTypeDef GPIO_InitStructure;
// CLOCK and MOSI Pins declaration
GPIO_InitStructure.GPIO_Pin = PIN_SCL|PIN_SI;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;
GPIO_Init(GPIOB, &GPIO_InitStructure);
// CS pin
GPIO_InitStructure.GPIO_Pin = PIN_CS|PIN_A0;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOB, &GPIO_InitStructure);
// SI & SCL = Alternate Functions
GPIO_PinAFConfig(GPIOB, GPIO_PinSource10, GPIO_AF_SPI2);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource15, GPIO_AF_SPI2);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource13, GPIO_AF_SPI2);
SPI_InitTypeDef SPI_InitStruct;
SPI_I2S_DeInit(SPI2);
SPI_InitStruct.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitStruct.SPI_Mode = SPI_Mode_Master;
SPI_InitStruct.SPI_DataSize = SPI_DataSize_8b;
SPI_InitStruct.SPI_CPOL = SPI_CPOL_Low;
SPI_InitStruct.SPI_CPHA = SPI_CPHA_1Edge;
SPI_InitStruct.SPI_NSS = SPI_NSS_Soft;
SPI_InitStruct.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2;
SPI_InitStruct.SPI_FirstBit = SPI_FirstBit_MSB;
SPI_InitStruct.SPI_CRCPolynomial = 7;
SPI_Init(SPI2, &SPI_InitStruct);
SPI_Cmd(SPI2, ENABLE);
With SPI_BaudRatePrescaler_2 : The screen works almost everytime
With SPI_BaudRatePrescaler_4 :The screen works half the time
With SPI_BaudRatePrescaler_8 :
The screen never works
So how can I increase the SPI speed, in order to try to solve my problem ?2013-12-19 06:53 AM
Hi
I think you are jumping to the wrong conclusion - that the problem is the SPI speed. ''Sometimes, when I power on my board, the screen have troubles to be initialized
'' ''The max SPI clock speed of the screen controller is 20MHz.
'' You should be able to configure the SPI for 20MHz. (Do not ask me - I have not work with the SPI peripheral yet) ''With SPI_BaudRatePrescaler_2 : The screen works almost everytime
With SPI_BaudRatePrescaler_4 :The screen works half the time
With SPI_BaudRatePrescaler_8 :
The screen never works
'' This tell me that the screen can work at theSPI_BaudRatePrescaler_4
speed. However, sometimes there is something during the start up that causes a problem. What voltage does theDOGM128
work at? (Some STM32 can work on as little as 1.8V - so it can start to boot at 1.8V) What is the start up time for theDOGM128
? What is the boot up time for the STM32 ? What reset circuit do you have for the STM32 ? Do you have an oscilloscope to look at what is happening during the bootup on the SPI?2013-12-20 06:17 AM
Hello, thanks for the reply !
- The DOGM128 voltage is 3.3V, like the STM32F4- I have no idea of the start up time of the screen, I can't find this information in the controller datasheet.- The hardware BOOT circuit is a divider bridge (the top resistor is 10K and the bottom is 510R). This is what you call a reset circuit ? In fact, I don't code anything with this BOOT pin, I have to ?- My oscilloscope is not enought powerfull to see the SPI messages, the speed is too high.I had a large delay before the screen init but it change nothing...2013-12-20 07:34 AM
I worked with an LCD DOGM128 but with texas stellaris micro. I don't remember well but my SPI speed was 10Mhz
My personal opinion: slowing down the clock should work better On top of my lcd init code I have this reset sequence.LCD_RST_PIN _LOW
wait 5ms LCD_RST_PIN _HIGH wait 5ms and then start the registers init procedure.2013-12-20 07:43 AM
Thanks !
Unfortunately my RESET pin is directly connected to the 3.3V, I was thinking it's an optionnal pin. But I hope there is another way to resolve my problem...In many examples on the internet the RESET pin is optionnal. So I think this is not the solution.2013-12-23 06:32 AM
Can I reiterate my question, How to know and how to change the SPI speed ?
I think that the SPI2 clock is based on APB2 frequency, but I'm unable to find APB2 frequency...Thanks !2013-12-23 08:38 AM
Hi
''Unfortunately my RESET pin is directly connected to the 3.3V'' Are you sure that the STM32 is starting correctly every time? Check the data sheet (the one for the electronics design) but I think most designs have at least a capacitor on the nreset, usually a resistor and capacitor. If you LEDs, can you have then toggling so that you can see the STM32 is working when it power up.2013-12-25 07:02 AM
Yes I'm sure that my STM32F4 start correctly everytime because everything works (UART, LEDS, input pins, I2C, USB...) even when the screen is not initialized.
2013-12-26 01:55 AM
I'm NOT sure the
reset pin
is
the problem but from the LCD controller manual (Ver1.5 pag.51)
Looking at your
code
I
have a doubt
Have you addedRCC_APB1PeriphClockCmd(SPI2_CLK, ENABLE);
?
You use SPI2 and ask for APB2 but SPI2 clock in STM32F4 is APB1
the clock value depend on clock peripheral configuration
Internal oscillator or esternal crystal ? if external value ?
You have
edited the file
system_stm32f4xx.c
?If
you have not made
changes
,at the beginning
of the file
there is a
table
with
the values of the
prescaler
clocks
including
APB1
APB2
and
knowing the frequency
of your
clock source
can
calculate
the frequencies
APB1
APB
22013-12-27 12:54 PM
Thanks francescato,
I added RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE); but the problem is still here.True for the controller init procedure but a lot of examples on the internet don't use the reset PIN.I use a 8MHz external oscillator, and I think I made changes to system_stm32f4xx.c :#define PLL_M 8#define PLL_N 336
#define PLL_P 2
#define PLL_Q 7
SystemCoreClock = 168000000;
AHBPrescTable[16] = {0, 0, 0, 0, 0, 0, 0, 0, 1, 2, 3, 4, 6, 7, 8, 9};So the clock speed of the clock is :(Coreclock / APB1) / Prescaler(168000000 / 4) / 2 = 21 MHz ?