cancel
Showing results for 
Search instead for 
Did you mean: 

interrupt problem for dma in usart

mohamad_armoon
Associate III
Posted on March 12, 2014 at 17:01

hi clive. thanks for information. i completed my code for stm32f4 Discovery with your idea with the link that you put here. i think it should be worked , but it doesn't. what's your idea about my code???

thanks in advance

#include ''stm32f4xx.h''

void

RCC_Configuration(

void

)

{

/* --------------------------- System Clocks Configuration -----------------*/

/* USART2 clock enable */

RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);

/* GPIOA clock enable */

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);

/* DMA1 clock enable */

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA1, ENABLE);

}

void

GPIO_Configuration(

void

)

{

GPIO_InitTypeDef GPIO_InitStructure;

/*-------------------------- GPIO Configuration ----------------------------*/

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_Init(GPIOA, &GPIO_InitStructure);

/* Connect USART pins to AF */

GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_USART2);

}

void

init_LED()

{

GPIO_InitTypeDef GPIO_InitStructure;

/*-------------------------- GPIO Configuration ----------------------------*/

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_Init(GPIOD, &GPIO_InitStructure);

}

void

USART2_Configuration(

void

)

{

USART_InitTypeDef USART_InitStructure;

USART_InitStructure.USART_BaudRate = 9600;

USART_InitStructure.USART_WordLength = USART_WordLength_8b;

USART_InitStructure.USART_StopBits = USART_StopBits_1;

USART_InitStructure.USART_Parity = USART_Parity_No;

USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

USART_Init(USART2, &USART_InitStructure);

USART_Cmd(USART2, ENABLE);

}

uint8_t Rx_Buffer;

void

DMA_Rx_Configuration(

void

)

{

DMA_InitTypeDef DMA_InitStructure;

DMA_DeInit(DMA1_Stream5);

DMA_InitStructure.DMA_Channel = DMA_Channel_4;

DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;

// receive

DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&Rx_Buffer;

DMA_InitStructure.DMA_BufferSize = (uint16_t)

sizeof

(Rx_Buffer);

DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&USART2->DR;

DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte;

DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;

DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;

DMA_InitStructure.DMA_Priority = DMA_Priority_High;

DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable;

DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full;

DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;

DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;

DMA_Init(DMA1_Stream5, &DMA_InitStructure);

/* Enable the USART Rx DMA request */

USART_DMACmd(USART2, USART_DMAReq_Rx, ENABLE);

/* Enable DMA Stream Half Transfer and Transfer Complete interrupt */

DMA_ITConfig(DMA1_Stream5, DMA_IT_TC, ENABLE);

// DMA_ITConfig(DMA1_Stream5, DMA_IT_HT, ENABLE);

/* Enable the DMA RX Stream */

DMA_Cmd(DMA1_Stream5, ENABLE);

}

void

NVIC_Rx_Configuration(

void

)

{

NVIC_InitTypeDef NVIC_InitStructure;

/* Configure the Priority Group to 2 bits */

NVIC_PriorityGroupConfig(NVIC_PriorityGroup_2);

/* Enable the UART4 RX DMA Interrupt */

NVIC_InitStructure.NVIC_IRQChannel = DMA1_Stream5_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

}

void

DMA1_Stream5_IRQHandler(

void

)

{

/* Test on DMA Stream Transfer Complete interrupt */

if

(DMA_GetITStatus(DMA1_Stream5, DMA_IT_TCIF5))

{

/* Clear DMA Stream Transfer Complete interrupt pending bit */

DMA_ClearITPendingBit(DMA1_Stream5, DMA_IT_TCIF5);

DMA_Rx_Configuration();

}

}

int

main()

{

RCC_Configuration();

GPIO_Configuration();

USART2_Configuration();

DMA_Rx_Configuration();

NVIC_Rx_Configuration();

init_LED();

uint8_t temp = 0;

while

(1){

temp = Rx_Buffer ;GPIO_SetBits(GPIOD,GPIO_Pin_12);

while

(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);

USART_SendData(USART2,Rx_Buffer);

// Tx_Buffer = Rx_Buffer;

if

(temp > 0){

GPIO_SetBits(GPIOD,GPIO_Pin_13);

}

}

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0