2012-05-24 1:11 AM
Please, could you help me? with STM32F4xx.
But I think it's general problem with GNU linker.
I'm working on SW for colour graphical display application.
It works fine.
But I need to store some data to Flash after the program start.
I want allocate for this data all 16K Sector 1 in Flash area.
I have tried different ways but unsuccessfully.
My variable is
const unsigned
short
int
FlashArray[8192].
I have tried this:
const unsigned short
int
FlashArray[8192] __attribute__ ((at((uint32_t)0x08004000)));This doesn't work in GNU.
I have tried also this:
const
unsigned
short
int
FlashArray[8192]
__attribute__
((section(
''.flash_data_array''
)));
+
change in stm32_flash.ld:
/* Specify the memory areas */
MEMORY
{
FLASH0 (rx) : ORIGIN = 0x08000000, LENGTH = 16K
FLASH1 (rx) : ORIGIN = 0x08004000, LENGTH = 16K
FLASH2 (rx) : ORIGIN = 0x08008000, LENGTH = 992K
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
MEMORY_B1 (rx) : ORIGIN = 0x60000000, LENGTH = 0K
}
/* Define output sections */
SECTIONS
{
/* The startup code goes first into FLASH */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASH0
/* My new eeprom area in FLASH */
.flash_data_array :
{
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
. = ALIGN(4);
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
} >FLASH1
?
/* The program code and other data goes into FLASH */
.text :
{
. = ALIGN(4);
*(.text) /* .text sections (code) */
*(.text*) /* .text* sections (code) */
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
*(.glue_7) /* glue arm to thumb code */
*(.glue_7t) /* glue thumb to arm code */
*(.eh_frame)
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
_etext = .; /* define a global symbols at end of code */
} >FLASH2
...
But this doesn't work too.
I don't know what's wrong.
I have tried to found out it on internet, but without success.
Here I found out this problem has more people.
Can you help me how to allocate variable array to Sector1 in Flash
and how to prohibit this sector to other flash data?
#linker2015-09-15 8:17 AM
Hi. I have a question.
How can we set value and use the value from beta variable? thank you.2015-09-15 11:10 AM
Well you'd write to it like any other FLASH interaction, you'd erase the sector it's in and then write to the memory in question. It's rather slow and invasive, and not like writing data in RAM.
It should read it like any other variable, the linker/compiler knows where it is, and you can access the memory just like any other memory location in RAM, ROM or FLASH