2017-10-04 11:25 PM
Hi,
I´m using a STM32F469I_Eval and in the Examples provides with STM32Cube_FW_F4, I can see that there are some Linked Resources (FILES). If I edit the .project file there are something like that:
<link>
<name>Drivers/STM32F4xx_HAL_Driver/stm32f4xx_hal.c</name> <type>1</type> <locationURI> copy_PARENT1/Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal.c</locationURI> </link><link>
<name>Drivers/BSP/STM32469I_EVAL/stm32469i_eval.c</name> <type>1</type> <locationURI>copy_PARENT1/Drivers/BSP/STM32469I_EVAL/stm32469i_eval.c</locationURI> </link>But if I want to create my own project I only can create a Linked Resource (FOLDER). If I edit the .project there are something like that:
<link>
<name>HAL</name> <type>2</type> <location>C:/workspace/SystemWorkbenchForSTM32/STM32F4xx_HAL_Driver</location> </link><link>
<name>STM3246I_EVAL</name> <type>2</type> <location>C:/workspace/SystemWorkbenchForSTM32/STM32469I_EVAL</location> </link>How can I link a File Resource like does ST? (without editing the .project file) I can´t find this option in eclipse menus
Thanks in advance,
Sergio
Solved! Go to Solution.
2017-10-05 12:15 PM
Hello Sergio!
You can add a Linked File Resource as below.
Right click to folder that you want to add the file ->New->File.
Click 'Advanced' button.
Check 'Link to File in the File System' checkbox.
Click button 'browse'
And choose the file you want.
Regards
vf
2017-10-05 2:23 AM
I asked in System Workbench for STM32 Forum also
http://www.openstm32.org/forumthread5855
Still No Answer...
2017-10-05 12:15 PM
Hello Sergio!
You can add a Linked File Resource as below.
Right click to folder that you want to add the file ->New->File.
Click 'Advanced' button.
Check 'Link to File in the File System' checkbox.
Click button 'browse'
And choose the file you want.
Regards
vf
2017-10-13 2:27 AM
Hello,
Is it possible to add more than one file at a time?
Regards
Sergio
2017-10-13 4:00 PM
Hello,
I don't know a way to choose many files and to add at a time.
But by adding a folder, same way as file , adds also all the contents of the folder.
Regards.
vf