2011-11-25 03:58 AM
Is it possibile to program a firmware in a stm32f10x micro without a jtag linker?
Thanks in advance.2011-11-25 05:33 AM
Is it possibile to program a firmware in a stm32f10x micro without a jtag linker?
They should also support the USART1 serial protocol using the system boot rom. Selected by the BOOTx pins. Others support CAN/USB modes. The protocol is described in several documents, there are ''Flash Loader'' applications. http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/USER_MANUAL/CD00171488.pdf2011-12-04 05:49 AM
See
http://code.google.com/p/stm32flash/
for programing flash in STM32 chips via UART (and RS232). See Steve Meirowsky