cancel
Showing results for 
Search instead for 
Did you mean: 

How many alarms can i have with RTC in STM32F407VGT

Patrick Morwald
Associate II
Posted on October 06, 2017 at 11:52

Hi,

i need two precise alarms i can set on my STM32F4 which will also be save when only the Backup domain is powered by a small battery. How many alarms can i have on the RTC of STM32F4? What would be my other options?

Thanks,

Patrick

#stm32f4 #rtc #rtc-hal
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Szymon PANECKI
Senior III
Posted on October 06, 2017 at 15:57

Hello Patrick,

RTC in STM32F407VG MCU allows to have two alarms: Alarm A and Alarm B. In fact all devices from STM32F4 family have two alarms.

Regards

Szymon

Imen.D
ST Employee
Posted on October 06, 2017 at 16:16

Hello,

RTC ALARM (Alarm A, Alarm B). For more details, please have a look to the reference manual related to your product.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Patrick Morwald
Associate II
Posted on October 06, 2017 at 16:42

Ok thanks!