cancel
Showing results for 
Search instead for 
Did you mean: 

How it is possible to have the PA10 output on STM3210E-EVAL board?

jfong
Associate II
Posted on October 11, 2010 at 07:45

How it is possible to have the PA10 output on STM3210E-EVAL board?

2 REPLIES 2
kashif
Associate II
Posted on May 17, 2011 at 14:10

it is not a problem if it is connected with R1-Out PIN. there is a resistor R36 in between so your logic level wont be disturbed. you can see your output at connector-CN10 (PIN-8).

hope it helps. Regards

jfong
Associate II
Posted on May 17, 2011 at 14:10

But the R36 is 0-Ohm. Anyway, thanks for your help. At least it let me know I didn't miss anything. The ST should remind user in their readme file to remove this resistor.

    Best Regards,