cancel
Showing results for 
Search instead for 
Did you mean: 

How G-431B-ESC1 drives CAN & PWM communication?

GST
Associate

Hello ST,

I bought a G-431B-ESC1, wish to driven with CAN & PWM, but cannot figure it out .

I red the manual(UM2516) was written:

"The CAN interface is provided with transceiver on board and a termination resistor is provided and manageable by firmware. " (page 13/29)

and the only words mentioned about the "firmware" is on page (18-19):

"3. Generate and upload the firmware code into the STM32G431CB MCU with IDE tool available."

However, it is generated by MCSDK.

Since I have used MCSDK for a while and was awared that MCSDK doesn't support "Generating CAN code nor PWM code", and the code proves I am right.

Is there any "FIRMWARE" or code that aviable for drive the CAN & PWM module?

or my only option is writing my own code to drive the modules?

BR

George

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
SBurc.1
Associate II

Same here,

any solution by ST?